Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
resources:eval:user-guides:eval-adicup3029:reference_designs:demo_cn0410 [05 Jun 2018 14:50]
mirceac [Obtaining the Source Code]
resources:eval:user-guides:eval-adicup3029:reference_designs:demo_cn0410 [05 Jul 2018 14:05] (current)
mirceac
Line 1: Line 1:
-====== EVAL-CN0410-ARDZ Shield ======+====== EVAL-CN0410-ARDZ Shield ​Demo ======
  
 [[ADI>​CN0410]] is an Arduino compatible shield that is optimized for smart agriculture to control current passing through LED's. The [[ADI>​CN0410]] is used along the the CFTL-LED Bar that has LED's with specific wavelengths that plants utilize. [[ADI>​CN0410]] is an Arduino compatible shield that is optimized for smart agriculture to control current passing through LED's. The [[ADI>​CN0410]] is used along the the CFTL-LED Bar that has LED's with specific wavelengths that plants utilize.
resources/eval/user-guides/eval-adicup3029/reference_designs/demo_cn0410.txt · Last modified: 05 Jul 2018 14:05 by mirceac