Wiki

This version is outdated by a newer approved version.DiffThis version (05 Jul 2018 14:05) was approved by Mircea Caprioru.The Previously approved version (05 Jun 2018 14:50) is available.Diff

This is an old revision of the document!


EVAL-CN0410-ARDZ Shield Demo

CN0410 is an Arduino compatible shield that is optimized for smart agriculture to control current passing through LED's. The CN0410 is used along the the CFTL-LED Bar that has LED's with specific wavelengths that plants utilize.


The circuit shown below is a complete 3-channel single-supply, 16-bit unbuffered voltage output DAC that maintains ±2 LSB integral and differential nonlinearity by utilizing a CMOS DAC. This circuit has a voltage to current conversion that controls the amount of current passing through an LED by using a MOSFET in its configuration. The circuit also has an isoSPI repeater that allows multiple boards to be controlled with a single master.



Demo Requirements

The following is a list of items needed in order to replicate this demo.

  • Hardware
    • EVAL-ADICUP3029
    • EVAL-CN0410-ARDZ
    • Mirco USB to USB cable
    • PC or Laptop with a USB port
  • Software
    • ADICUP3029_demo_CN0410 software
    • CrossCore Embedded Studio (2.6.0 or higher)
    • ADuCM302x DFP (2.0.0 or higher)
    • ADICUP3029 BSP (1.0.0 or higher)
    • Serial Terminal Program (Required for running in release mode only)
      • Such as Putty or Tera Term

Setting up the Hardware

Chip Select

The chip select pin of the AD5686 is hardware configurable and routed to 3 general purpose I/O pins on the board. Use the table below to change the location of the chip select simply by moving the shunt on P21, and ensuring the software is configured the same way. By default the chip select is located on GPIO 8. This feature allows multiple boards using SPI communications protocol to be stacked on top of each other.

Chip Select (P21) GPIO (P16)
Pins 1 & Pin 2 GPIO 8
Pins 3 & Pin 4 GPIO 9
Pins 5 & Pin 6 GPIO 10

Configuring the Software

The software for EVAL-CN0410 does not require any particular configurations in order to setup the application. The only setting that the user could make would be the selection of the CS pin. This can be done by modifying the SYNC_PORT and SYNC_PIN inside adi_cn0410.h.

#define SYNC_PORT	ADI_GPIO_PORT1 //this is the CS pin
#define SYNC_PIN	ADI_GPIO_PIN_12

Outputting Data

After the application starts the user can send commands to set the output of the DAC channels. Available commands:

  • set_a value
  • set_b value
  • set_c value
  • set_zero - resets all channels to 0

The value can be between 0 and 65535.

Serial Terminal Output

Once the hardware and software is configured, user needs to follow on screen instructions to run EVAL-CN0410 demo.

Following is the UART configuration.

  Select COM Port
  Baud rate: 9600
  Data: 8 bit
  Parity: none
  Stop: 1 bit
  Flow Control: none


Obtaining the Source Code

We recommend not opening the project directly, but rather import it into CrossCore Embedded Studios and make a local copy in your workspace.

The source code and include files of the ADuCM3029_demo_cn0410 can be found here:

How to use the Tools

The official tool we promote for use with the EVAL-ADICUP3029 is CrossCore Embedded Studio. For more information on downloading the tools and a quick start guide on how to use the tool basics, please check out the Tools Overview page.

Importing

For more detailed instructions on importing this application/demo example into the CrossCore Embedded Studios tools, please view our How to import existing projects into your workspace section.

Debugging

For more detailed instructions on importing this application/demo example into the CrossCore Embedded Studios tools, please view our How to configure the debug session section.

Project Structure

The project is structured in 3 sections :

  • source - that contains the communication, timer and main sections
  • include - header files
  • sensors - with DAC driver

End of Document

resources/eval/user-guides/eval-adicup3029/reference_designs/demo_cn0410.1530792327.txt.gz · Last modified: 05 Jul 2018 14:05 by Mircea Caprioru