Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
resources:eval:user-guides:eval-adicup3029:reference_designs:demo_cn0401 [03 Jan 2021 21:55]
Robin Getz fix links
resources:eval:user-guides:eval-adicup3029:reference_designs:demo_cn0401 [08 Mar 2021 01:18]
Zuedmar Arceo [Obtaining the Source Code] adding in .Hex files
Line 133: Line 133:
  
  
-===== Obtaining the Source Code =====+===== Obtaining the Software ​=====
  
-We recommend not opening ​the project directly, but rather import it into CrossCore Embedded Studios ​and make a local copy in your workspace+There are two basic ways to program ​the ADICUP3029 with the software for the CN0401. 
 +  - Dragging ​and Dropping the .Hex to the Daplink drive 
 +  - Building, Compiling, and Debugging using CCES
  
-The source code and include files of the **ADuCM3029_demo_cn0401** can be found here:+Using the drag and drop method, ​the software is going to be a version that Analog Devices creates for testing and evaluation purposes. ​ This is the EASIEST way to get started with the reference design
  
-<WRAP round 80% download>+Importing the project into CrossCore is going to allow you to change parameters and customize the software to fit your needs, but will be a bit more advanced and will require you to download ​the CrossCore toolchain.  ​
  
-[[https://​github.com/​analogdevicesinc/​EVAL-ADICUP3029/​tree/​master/​projects/​ADuCM3029_demo_cn0401| ​ADuCM3029_demo_cn0401 at Github]]+The software for the **ADuCM3029_demo_cn0401** can be found here: 
 + 
 +<WRAP round 80% download>​ 
 +Prebuilt CN0401 Hex File 
 +  * [[https://​github.com/​analogdevicesinc/​EVAL-ADICUP3029/​releases/​download/​Latest/​ADuCM3029_demo_cn0401.hex| AduCM3029_demo_cn0401.Hex]] 
 +Complete CN0401 Source Files 
 +  * [[https://​github.com/​analogdevicesinc/​EVAL-ADICUP3029/​tree/​master/​projects/​ADuCM3029_demo_cn0401| ​AduCM3029_demo_cn0401 Source Code]]
    
 </​WRAP>​ </​WRAP>​
resources/eval/user-guides/eval-adicup3029/reference_designs/demo_cn0401.txt · Last modified: 08 Mar 2021 01:18 by Zuedmar Arceo