Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
resources:eval:user-guides:eval-adicup3029:reference_designs:demo_cn0397 [20 Jul 2017 20:49]
Brandon added more step by step details
resources:eval:user-guides:eval-adicup3029:reference_designs:demo_cn0397 [10 Jan 2018 18:13] (current)
Brandon
Line 16: Line 16:
  
  
- The 16-bits ADC data are received using **SPI interface** of the EVAL-ADICUP360 ​board. The **UART interface** (**9600** baud rate and **8-bits** data length) is used to send(and to receive) data to (from) a terminal window.+ The 16-bits ADC data are received using **SPI interface** of the EVAL-ADICUP3029 ​board. The **UART interface** (**9600** baud rate and **8-bits** data length) is used to send(and to receive) data to (from) a terminal window.
  
 **Light intensity** [Lux] is calculated using ADC output value for selected channel and a constant value for each color: **Light intensity** [Lux] is calculated using ADC output value for selected channel and a constant value for each color:
Line 61: Line 61:
 ===== Configuring the Software ===== ===== Configuring the Software =====
  
-In the //cn0398_app.h// header files you can configure the following parameters:+In the //cn0397_app.h// header files you can configure the following parameters:
 \\ \\
     * **ADI_APP_DISPATCH_TIMEOUT** - //DISPATCH TIMEOUT// will define how often the data is sent over Bluetooth.     * **ADI_APP_DISPATCH_TIMEOUT** - //DISPATCH TIMEOUT// will define how often the data is sent over Bluetooth.
resources/eval/user-guides/eval-adicup3029/reference_designs/demo_cn0397.txt · Last modified: 10 Jan 2018 18:13 by Brandon