This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:eval:user-guides:eval-adicup3029:reference_designs:demo_cn0397 [20 Jul 2017 20:49] – added more step by step details Brandon Bushey | resources:eval:user-guides:eval-adicup3029:reference_designs:demo_cn0397 [10 Jan 2018 18:13] – Brandon Bushey | ||
---|---|---|---|
Line 16: | Line 16: | ||
- | The 16-bits ADC data are received using **SPI interface** of the EVAL-ADICUP360 | + | The 16-bits ADC data are received using **SPI interface** of the EVAL-ADICUP3029 |
**Light intensity** [Lux] is calculated using ADC output value for selected channel and a constant value for each color: | **Light intensity** [Lux] is calculated using ADC output value for selected channel and a constant value for each color: | ||
Line 61: | Line 61: | ||
===== Configuring the Software ===== | ===== Configuring the Software ===== | ||
- | In the //cn0398_app.h// header files you can configure the following parameters: | + | In the //cn0397_app.h// header files you can configure the following parameters: |
\\ | \\ | ||
* **ADI_APP_DISPATCH_TIMEOUT** - //DISPATCH TIMEOUT// will define how often the data is sent over Bluetooth. | * **ADI_APP_DISPATCH_TIMEOUT** - //DISPATCH TIMEOUT// will define how often the data is sent over Bluetooth. |