Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Next revision
Previous revision
resources:eval:user-guides:eval-adicup3029:reference_designs:demo_blink [30 May 2017 23:01]
Brandon Bushey file names, working
resources:eval:user-guides:eval-adicup3029:reference_designs:demo_blink [23 Nov 2022 16:27] (current)
Brandon Bushey updating to use the Github project versus the BSP project
Line 1: Line 1:
-====== Blink LED (ADICUP3029) ​Demo======+====== Blink LED Demo======
  
-The **ADICUP3029_Blink** is a Blink LED demo project for the **EVAL-ADICUP3029** base board which is created using the Analog Devices Cross Core Embedded Studio.+The **ADuCM3029_Blink** is a Blink LED demo project for the **EVAL-ADICUP3029** base board which is created using the Analog Devices Cross Core Embedded Studio.
  
  
 ===== General Description/​Overview ===== ===== General Description/​Overview =====
  
-The **ADICUP3029_Blink** project uses [[http://​www.analog.com/​en/​design-center/​evaluation-hardware-and-software/​evaluation-boards-kits/​eval-adicup3029.html| EVAL-ADICUP3029]] which is an Ultra Low Power, Arduino compatible ARM Cortex M3 based platform. The platform support various sensor shields.+The **ADuCM3029_Blink** project uses [[adi>en/​design-center/​evaluation-hardware-and-software/​evaluation-boards-kits/​eval-adicup3029.html| EVAL-ADICUP3029]] which is an Ultra Low Power, Arduino compatible ARM Cortex M3 based platform. The platform support various sensor shields.
    
 +===== Demo Requirements ​ =====
 +
 +The following is a list of items needed in order to replicate this demo.
 +  * Hardware
 +    * EVAL-ADICUP3029
 +    * Mirco USB to USB cable
 +    * PC or Laptop with a USB port
 +  * Software
 +    * CrossCore Embedded Studio (2.6.0 or higher)
 +    * ADuCM302x DFP (2.0.0 or higher)
 +
 ===== Setting up the Hardware ===== ===== Setting up the Hardware =====
 No specific hardware setup required for this demo No specific hardware setup required for this demo
Line 21: Line 32:
 ===== Obtaining the Source Code ===== ===== Obtaining the Source Code =====
  
-We recommend not opening the project directly, but rather use CrossCore Embedded Studio (CCES) example browse to open the project. Below screen shot shows how to open project from CCES Example browser. +The source code and include files of the **ADuCM3029_Blink** demo can be found here:
- +
-{{:​resources:​eval:​user-guides:​eval-adicup3029:​reference_designs:​blinky_selection.png?​920|}} +
- +
- +
- +
-The source code and include files of the **ADICUP3029_Blink** demo can be found here:+
  
 <WRAP round 80% download>​ <WRAP round 80% download>​
-<fc #ff0000>**ADD GITHUB LINK HERE!**</fc>  ​+[[repono-OS/tree/​master/​projects/​aducm_blinky_example]]
 </​WRAP>​ </​WRAP>​
  
Line 45: Line 50:
  
 For more detailed instructions on importing this application/​demo example into the CrossCore Embedded Studios tools, please view our [[resources:​eval:​user-guides:​eval-adicup3029:​tools:​cces_user_guide#​how_to_configure_the_debug_session_for_an_aducm3029_application|How to configure the debug session]] section. For more detailed instructions on importing this application/​demo example into the CrossCore Embedded Studios tools, please view our [[resources:​eval:​user-guides:​eval-adicup3029:​tools:​cces_user_guide#​how_to_configure_the_debug_session_for_an_aducm3029_application|How to configure the debug session]] section.
- 
-==== Project Structure ==== 
- 
-The **ADICUP3029_Blink** is a C project that uses ADuCM3029 C/C++ Project structure. ​ 
-  
-{{:​resources:​eval:​user-guides:​eval-adicup3029:​reference_designs:​blinky_projdirectory.png?​700|}} 
-\\ 
-blinky_example.c and blinky_example.h are the main source and header files related to **ADICUP3029_Blink** be found under Source folder. 
  
 // End of Document // // End of Document //
  
  
resources/eval/user-guides/eval-adicup3029/reference_designs/demo_blink.1496178096.txt.gz · Last modified: 30 May 2017 23:01 by Brandon Bushey