Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Next revision
Previous revision
resources:eval:user-guides:eval-adicup3029:reference_designs:demo_blink [29 May 2017 05:25]
Srinivas Gollakota created
resources:eval:user-guides:eval-adicup3029:reference_designs:demo_blink [23 Nov 2022 16:27] (current)
Brandon Bushey updating to use the Github project versus the BSP project
Line 1: Line 1:
-====== Blink LED (ADICUP3029) ​Demo======+====== Blink LED Demo======
  
-The **ADICUP3029_Blink** is a Blink LED demo project for the **EVAL-ADICUP3029** base board which is created using the Analog Devices Cross Core Embedded Studio.+The **ADuCM3029_Blink** is a Blink LED demo project for the **EVAL-ADICUP3029** base board which is created using the Analog Devices Cross Core Embedded Studio.
  
  
 ===== General Description/​Overview ===== ===== General Description/​Overview =====
  
-The **ADICUP3029_Blink** project uses [[http://​www.analog.com/​en/​design-center/​evaluation-hardware-and-software/​evaluation-boards-kits/​eval-adicup3029.html| EVAL-ADICUP3029]] which is an Ultra Low Power, Arduino compatible ARM Cortex M3 based platform. The platform support various sensor shields.+The **ADuCM3029_Blink** project uses [[adi>en/​design-center/​evaluation-hardware-and-software/​evaluation-boards-kits/​eval-adicup3029.html| EVAL-ADICUP3029]] which is an Ultra Low Power, Arduino compatible ARM Cortex M3 based platform. The platform support various sensor shields.
    
 +===== Demo Requirements ​ =====
 +
 +The following is a list of items needed in order to replicate this demo.
 +  * Hardware
 +    * EVAL-ADICUP3029
 +    * Mirco USB to USB cable
 +    * PC or Laptop with a USB port
 +  * Software
 +    * CrossCore Embedded Studio (2.6.0 or higher)
 +    * ADuCM302x DFP (2.0.0 or higher)
 +
 ===== Setting up the Hardware ===== ===== Setting up the Hardware =====
 No specific hardware setup required for this demo No specific hardware setup required for this demo
Line 21: Line 32:
 ===== Obtaining the Source Code ===== ===== Obtaining the Source Code =====
  
-We recommend not opening the project directly, but rather use CCES example browse to open the project. Below screen shot shows how to open project from CCES Example browser. +The source code and include files of the **ADuCM3029_Blink** demo can be found here:
- +
-{{:​resources:​eval:​user-guides:​eval-adicup3029:​reference_designs:​blinky_selection.png?​920|}} +
- +
- +
- +
-The source code and include files of the **ADICUP3029_Blink** demo can be found here:+
  
 <WRAP round 80% download>​ <WRAP round 80% download>​
-<fc #ff0000>**ADD GITHUB LINK HERE!**</fc>  ​+[[repono-OS/tree/​master/​projects/​aducm_blinky_example]]
 </​WRAP>​ </​WRAP>​
  
Line 45: Line 50:
  
 For more detailed instructions on importing this application/​demo example into the CrossCore Embedded Studios tools, please view our [[resources:​eval:​user-guides:​eval-adicup3029:​tools:​cces_user_guide#​how_to_configure_the_debug_session_for_an_aducm3029_application|How to configure the debug session]] section. For more detailed instructions on importing this application/​demo example into the CrossCore Embedded Studios tools, please view our [[resources:​eval:​user-guides:​eval-adicup3029:​tools:​cces_user_guide#​how_to_configure_the_debug_session_for_an_aducm3029_application|How to configure the debug session]] section.
- 
-==== Project Structure ==== 
- 
-The **ADICUP3029_ADXL362** is a C project that uses ADuCM3029 C/C++ Project structure. ​ 
-  
-This project contains: system initialization part - disabling watchdog, setting system clock, enabling clock for peripherals;​ port configuration for SPI read/write; configuring and reading from ADXL362, UART read/write functions; 
- 
-{{:​resources:​eval:​user-guides:​eval-adicup3029:​reference_designs:​blinky_projdirectory.png?​700|}} 
-\\ 
-blinky_example.c and blinky_example.h are the main source and header files related to **ADICUP3029_Blink** be found under Source folder. 
- 
  
 // End of Document // // End of Document //
  
  
resources/eval/user-guides/eval-adicup3029/reference_designs/demo_blink.1496028304.txt.gz · Last modified: 29 May 2017 05:25 by Srinivas Gollakota