This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:eval:user-guides:eval-adicup3029:reference_designs:demo_blink [30 May 2017 23:01] – file names, working Brandon Bushey | resources:eval:user-guides:eval-adicup3029:reference_designs:demo_blink [31 May 2017 22:33] – added demo requirements Brandon Bushey | ||
---|---|---|---|
Line 8: | Line 8: | ||
The **ADICUP3029_Blink** project uses [[http:// | The **ADICUP3029_Blink** project uses [[http:// | ||
+ | ===== Demo Requirements | ||
+ | |||
+ | The following is a list of items needed in order to replicate this demo. | ||
+ | * Hardware | ||
+ | * EVAL-ADICUP3029 | ||
+ | * Mirco USB to USB cable | ||
+ | * PC or Laptop with a USB port | ||
+ | * Software | ||
+ | * CrossCore Embedded Studio (2.6.0 or higher) | ||
+ | * ADuCM302x DFP (2.0.0 or higher) | ||
+ | * ADICUP3029 BSP (1.0.0 or higher) | ||
+ | |||
===== Setting up the Hardware ===== | ===== Setting up the Hardware ===== | ||
No specific hardware setup required for this demo | No specific hardware setup required for this demo |