This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
resources:eval:user-guides:eval-adicup3029:reference_designs:demo_blink [30 May 2017 23:01] – file names, working Brandon Bushey | resources:eval:user-guides:eval-adicup3029:reference_designs:demo_blink [23 Nov 2022 16:23] – [Obtaining the Source Code] updated to no-os repo for project files Brandon Bushey | ||
---|---|---|---|
Line 6: | Line 6: | ||
===== General Description/ | ===== General Description/ | ||
- | The **ADICUP3029_Blink** project uses [[http:// | + | The **ADICUP3029_Blink** project uses [[adi>en/ |
+ | ===== Demo Requirements | ||
+ | |||
+ | The following is a list of items needed in order to replicate this demo. | ||
+ | * Hardware | ||
+ | * EVAL-ADICUP3029 | ||
+ | * Mirco USB to USB cable | ||
+ | * PC or Laptop with a USB port | ||
+ | * Software | ||
+ | * CrossCore Embedded Studio (2.6.0 or higher) | ||
+ | * ADuCM302x DFP (2.0.0 or higher) | ||
+ | * ADICUP3029 BSP (1.0.0 or higher) | ||
+ | |||
===== Setting up the Hardware ===== | ===== Setting up the Hardware ===== | ||
No specific hardware setup required for this demo | No specific hardware setup required for this demo | ||
Line 21: | Line 33: | ||
===== Obtaining the Source Code ===== | ===== Obtaining the Source Code ===== | ||
- | We recommend not opening the project directly, but rather use CrossCore Embedded Studio (CCES) example browse to open the project. Below screen shot shows how to open project from CCES Example browser. | + | The source code and include files of the **ADuCM3029_Blink** demo can be found here: |
- | + | ||
- | {{: | + | |
- | + | ||
- | + | ||
- | + | ||
- | The source code and include files of the **ADICUP3029_Blink** demo can be found here: | + | |
<WRAP round 80% download> | <WRAP round 80% download> | ||
- | <fc #ff0000>**ADD GITHUB LINK HERE!**</fc> | + | [[repo> no-OS/tree/ |
</ | </ | ||