This shows you the differences between two versions of the page.
Both sides previous revision Previous revision Next revision | Previous revision | ||
resources:eval:user-guides:eval-adicup3029:reference_designs:demo_adxrs290_pmod [10 Mar 2021 03:54] Zuedmar Arceo [Outputting Data] |
resources:eval:user-guides:eval-adicup3029:reference_designs:demo_adxrs290_pmod [15 Mar 2021 05:18] Zuedmar Arceo |
||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== ADXRS290 Gyroscope PMOD Demo ====== | + | ====== ADXRS290 Gyroscope PMOD Command Line Interface Demo ====== |
The **ADuCM3029_demo_adxrs290** is a dual-axis angular rate sensor (gyroscope) demo project | The **ADuCM3029_demo_adxrs290** is a dual-axis angular rate sensor (gyroscope) demo project | ||
Line 61: | Line 61: | ||
There are two basic ways to program the ADICUP3029 with the software for the ADXRS290. | There are two basic ways to program the ADICUP3029 with the software for the ADXRS290. | ||
- Dragging and Dropping the .Hex to the Daplink drive | - Dragging and Dropping the .Hex to the Daplink drive | ||
- | - Building, Compiling, and Debugging using CCES | + | - Building, Compiling, and Debugging using CCES\\ |
+ | Using the drag and drop method, the software is going to be a version that Analog Devices creates for testing and evaluation purposes. This is the EASIEST way to get started with the reference design. | ||
Importing the project into CrossCore is going to allow you to change parameters and customize the software to fit your needs, but will be a bit more advanced and will require you to download the CrossCore toolchain. | Importing the project into CrossCore is going to allow you to change parameters and customize the software to fit your needs, but will be a bit more advanced and will require you to download the CrossCore toolchain. |