This is an old revision of the document!
This demo will use EVAL-ADXL372-ARDZ along with EVAL-ADICUP3029 to create a impact measurement application. The ADXL372 is an ultralow power, 3-axis, ±200 g MEMS accelerometer.
The ADXL372 demo project uses the EVAL-ADXL372-ARDZ shield which has an ADXL372 accelerometer and a incorporated NHD-C12832A1Z-NSW-BBW display (128×32). However, for this example the display is not used.
The EVAL-ADICUP3029 is designed for IOT (Internet of Things) applications in mind, and therefore comes with on board Bluetooth 5.0 module.
Set switch S2 to USB Arduino function in order to view data over UART also. The UART baud rate is 9600 baud.
Place the EVAL-ADXL372-ARDZ on top of the EVAL-ADICUP3029. Make sure the jumpers P8, P9, P6 are configured exactly as the picture above.
After making these configurations just plug in the USB connector.