This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:eval-adicup3029:reference_designs:demo_adxl362 [14 Jan 2021 05:23] – use / interwiki links Robin Getz | resources:eval:user-guides:eval-adicup3029:reference_designs:demo_adxl362 [08 Mar 2021 07:21] (current) – [Obtaining the Source Code] adding in .Hex files Zuedmar Arceo | ||
---|---|---|---|
Line 36: | Line 36: | ||
- Plug the USB cable | - Plug the USB cable | ||
- | ===== Obtaining the Source Code ===== | + | ===== Obtaining the Software |
- | Details of how to create an Adicup3029 project from sources can be found here: | + | There are two basic ways to program the ADICUP3029 with the software for the ESP8266. |
- | https:// | + | - Dragging and Dropping the .Hex to the Daplink drive |
+ | | ||
- | The source code and include files of the **ADuCM3029_demo_esp8266** can be found here: | + | Using the drag and drop method, |
- | <WRAP round 80% download> | + | Importing the project into CrossCore is going to allow you to change parameters and customize the software to fit your needs, but will be a bit more advanced and will require you to download |
- | [[https:// | + | The software for the **ADuCM3029_demo_esp8266** can be found here: |
+ | <WRAP round 80% download> | ||
+ | Prebuilt ESP8266 Hex File | ||
+ | * [[https:// | ||
+ | Complete ESP8266 Source Files | ||
+ | * [[https:// | ||
+ | |||
</ | </ | ||