This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:eval-adicup3029:reference_designs:demo_adt7420 [03 Mar 2021 09:41] – [Obtaining the Source Code] adding in .Hex files Zuedmar Arceo | resources:eval:user-guides:eval-adicup3029:reference_designs:demo_adt7420 [14 Mar 2021 06:04] (current) – [Obtaining the Source Code] adding in .Hex files Zuedmar Arceo | ||
---|---|---|---|
Line 125: | Line 125: | ||
- Dragging and Dropping the .Hex to the Daplink drive | - Dragging and Dropping the .Hex to the Daplink drive | ||
- Building, Compiling, and Debugging using CCES | - Building, Compiling, and Debugging using CCES | ||
+ | |||
+ | Using the drag and drop method, the software is going to be a version that Analog Devices creates for testing and evaluation purposes. | ||
Importing the project into CrossCore is going to allow you to change parameters and customize the software to fit your needs, but will be a bit more advanced and will require you to download the CrossCore toolchain. Below screen shot shows how to open project from CCES Example browser. | Importing the project into CrossCore is going to allow you to change parameters and customize the software to fit your needs, but will be a bit more advanced and will require you to download the CrossCore toolchain. Below screen shot shows how to open project from CCES Example browser. | ||
Line 136: | Line 138: | ||
<WRAP round 80% download> | <WRAP round 80% download> | ||
Prebuilt ADT7420 Hex File | Prebuilt ADT7420 Hex File | ||
- | * [[ resources:eval:user-guides: | + | * [[https:// |
Complete ADT7420 Source Files | Complete ADT7420 Source Files | ||
- | * [[https:// | + | * [[https:// |
</ | </ | ||