There have been several enclosures made for the EVAL-ADICUP3029, and even some for the EVAL-ADICUP3029 and attachable daughter boards. I have put together a table of the current 3D printable cases we have to date. If you have created a 3D case for the ADICUP3029 and would like to have it added to this table, please do so. We will review your submission and work on adding it to the list.
If you would like to view the designs in a 3D environment to get a better idea of what the design looks like, there are many free STL viewers that exist on the internet. I've provided a link below to the one that I think is the easiest to use, you can simply drag and drop the STL files into the browser.
These 3D printer STL files were made by community contributors as additional collateral to the ADICUP3029 ecosystem. Analog Devices is NOT responsible for 3D files that print incorrectly or are not compatible with your particular printer. It is up to the user to make sure the enclosures can be printed on their machines.
3D STL File | Boards Intended for Case | Description | Picture |
---|---|---|---|
ADICUP3029 Case 1 | EVAL-ADICUP3029 | * Used for ADICUP3029 board and PMOD add on boards. * Three-sided case that you slide the ADICUP3029 into. | ![]() |
ADICUP3029 Case 1 with CN0357 Cutout | EVAL-ADICUP3029 EVAL-CN0357-ARDZ | * Used for ADICUP3029 board, PMOD add on boards, and the CN0357 shield. * Three-sided case that you slide the hardware stack up into. | ![]() |
ADICUP3029 Bottom Plate | EVAL-ADICUP3029 | * Used for ADICUP3029 board, PMOD add on boards, and any shield. * Bottom only case, with mounting holes for the ADICUP3029. * Stack any shields or PMODs using this case. | ![]() |
ADICUP3029 Bottom Plate with Battery Pack Cutout | EVAL-ADICUP3029 | * Used for ADICUP3029 board, PMOD add on boards, and any shield. * Bottom only case, with mounting holes and battery pack access for the ADICUP3029. * Stack any shields or PMODs using this case. | ![]() |