Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
resources:eval:user-guides:eval-adbms6830bmsw:software [27 Feb 2024 00:58] – minor edits Joyce Velascoresources:eval:user-guides:eval-adbms6830bmsw:software [06 Mar 2024 09:05] (current) – [Installing the Firmware] Celso Aron
Line 32: Line 32:
 <hidden **Click here for instructions on how to flash the firmware image using the MAX32625PICO** > <hidden **Click here for instructions on how to flash the firmware image using the MAX32625PICO** >
  
-  - Access the [[https://github.com/analogdevicesinc/max32626pico-firmware-images|MAX32625PICO Firmware Repository]] and download the image for the specific MCU (e.g., MAX32690).+  - Access the [[https://github.com/analogdevicesinc/max32625pico-firmware-images|MAX32625PICO Firmware Repository]] and download the image for the specific MCU (e.g., MAX32690).
   - Do not connect the MAX32625PICO from the PC and the MCU board that you are using (e.g., AD-APARDMAX32690-SL, MAX32670 MCU base board).   - Do not connect the MAX32625PICO from the PC and the MCU board that you are using (e.g., AD-APARDMAX32690-SL, MAX32670 MCU base board).
   - Plug the micro-USB cable only in the MAX32625PICO.   - Plug the micro-USB cable only in the MAX32625PICO.
resources/eval/user-guides/eval-adbms6830bmsw/software.txt · Last modified: 06 Mar 2024 09:05 by Celso Aron