Wiki

This version is outdated by a newer approved version.DiffThis version (30 Jul 2021 14:15) was approved by Bríde Ní Riagáin.The Previously approved version (30 Jul 2021 14:10) is available.Diff

This is an old revision of the document!


Thermocouple & Cold Junction Compensation Measurements with AD74413R

Introduction

The AD74413R is a quad channel software configurable I/O IC that provides multiple analog and digital functions to a single pair of screw terminals. The AD74413R is configured over a single SPI interface. The part offers Voltage/Current outputs, Voltage/Current Inputs, Digital Inputs and RTD/Thermocouple measurement capability. This Wiki page will focus on how a thermocouple can be measured along with a cold junction compensation measurement.


Refer to figure 1 for a high level block diagram of the required connections for thermocouple measurements.

The thermocouple generates a voltage that is proportional to the temperature difference between the measurement point and where the thermocouple is connected at the screw terminals, the cold junction. To be able to determine the temperature at the measurement point, the cold junction temperature must be measured along with the voltage generated by the thermocouple.
The thermocouple should be connected between the I/OP and I/ON screw terminals. The AD74413R can be configured in Voltage Input mode, with the ADC range set to the ±104.16mV to measure the small voltage generated by the Thermocouple measurements.
The AD74413R can support cold junction compensation measurements by measuring the response from an external thermistor resistor divider using the onboard diagnostics. The LVIN pin can be used to measure the thermistor voltage within an ADC range of 2.5V. The resistor divider can be placed close to the terminal pins where the thermocouple is connected.
The temperature at the thermocouple is calculated using a combination of the thermocouple and cold junction measurements.


Figure 1: AD74413R configured for thermocouple measurements

Implementation

Two measurement steps are taken to determine the temperature of the measurement point.
First, the cold junction temperature is measured to establish a reference point for the thermocouple. Figure 2 shows a snapshot from the AD74413R evaluation board. This circuit shows the implementation required to use the AD74413R to determine TCOLD_JUNC, the cold junction temperature:

  • The reference voltage to the AD74413R is applied to the top of a resistor divider. The resistor divider is made up of a 33kΩ resistor, R64 and a 33kΩ thermistor, RT1.
  • The resistance of the thermistor is proportional to the ambient temperature. The resultant voltage is measured from the tap-off point in the middle of the divider, which is connected to the LVIN pin. The LVIN pin can be measured by the ADC in a 2.5V range, which is set by the reference provided.
  • The resistance of the thermistor can be calculated from the measured ADC_CODE, using the following equation:

RRT1 = -(33000* ADC_CODE) / (ADC_CODE – 65535)


Figure 2: LVIN schematic configuration

The voltage generated by the thermocouple must also be measured.
Configure one of the AD74413R channels in Voltage input mode with the ADC range set to ±104.16mV. Connect the thermocouple to the I/OP & I/ON screw terminals. Calculate the thermocouple voltage using the following equation:

VADC=VMIN + ((ADC_CODE)/65535 × VoltageRange)

Where:
Vmin is the minimum of the ADC range, -104.16mV
ADC_CODE is the code measured by the ADC
VoltageRange is 208.32 mV

The voltage measured by the ADC can then be combined with the cold junction temperature to calculate the hot junction temperature:

TTC =(VADC/S)- TCOLD_JUNC

where:
TTC is the hot junction temperature
VADC is the voltage measured between the thermocouple terminals
TCOLD_JUNC is the cold junction temperature
S is the Seeback Coefficient, specific to the chosen thermocouple

Register Writes

The following is a set of register writes required to take thermocouple & cold junction temperature measurements.

  • Enable Voltage Input mode on Channel A and set ADC range to ±104.16mV
    • Write 0x0003 to CH_FUNC_SETUP register (address: 0x01)
    • Write 0x0080 to ADC_CONFIG register (address: 0x05)
  • Assign the LVIN pin to the Diagnostic 0 channel
    • Write 0x000E to the DIAG_ASSIGN register (address: 0x24)
  • Enable ADC for continuous conversions on Channel A and Diagnostic Channel 0.
    • Write 0x0211 to the ADC_CONV_CTRL register (address: 0x23) to enable continuous conversions on the ADC
  • Read ADC result (Thermocouple voltage) from ADC_RESULT register (address: 0x26)
    • Read the Diagnostic 0 result from the DIAG_RESULT register (address: 0x2A)



Open Wire Detect

To detect an open-wire on a connected thermocouple, the I/OP terminal can be connected to ground via an on-chip 200kΩ resistor. If the thermocouple lead is open, the terminal will instantly be pulled to 0V (or code midscale of the ADC) in the ±104.16mV range. This ground connection can be used periodically to check that the screw is not floating. To enable the 200kΩ to ground, set bit 2 in the ADC_CONFIG register (address 0x05 for channel A).

Back to other AD7441xR Wiki Topics

resources/eval/user-guides/eval-ad7441x/tools/thermocouple.1627647312.txt.gz · Last modified: 30 Jul 2021 14:15 by Bríde Ní Riagáin