Full-featured evaluation board multichannel, simultaneous sampling ADC On-board reference, reference buffer, and ADC driver On-board power supplies Board-compatible high-speed system demonstration platform EVAL-SDP-CH1Z (SDP-H1)) controller PC software for control and data analysis
EVAL-AD7386FMCZ evaluation board Instructions to download software
EVAL-SDP-CH1Z Signal source PC running Windows XP SP3, Windows Vista, Windows 7, or Windows 10 with a USB port
ACE evaluation software AD738x ACE plugin
The EVAL-AD7386FMCZ is a full-featured evaluation board designed to evaluate all the features of the AD7386 analog-to-digital converter (ADC). The evaluation board can be controlled by the EVAL-SDP-CH1Z via the 160-way system demonstration platform connector, P7. The EVAL-SDP-CH1Z board controls the evaluation board through the USB port of the PC using the Analysis Control Evaluation (ACE]) software, which is available for download from the ACE software page.
The EVAL-AD7386FMCZ can evaluate the [[adi>AD7387, AD7388, AD4684, and AD4685by using the AD738x ACE plugin found on the EVAL-AD7386FMCZ product page. The only difference is the number of SCLKs that clock out the conversion results, which is dependent on the resolution for each generic.
Complete specifications for the AD7386/AD7387/AD7388/AD4684/AD4685are provided in the AD7386/AD7387/AD7388/AD4684/AD4685datasheet. Consult these specifications in conjunction with this user guide when using the evaluation board. Full details on the EVAL-SDP-CH1Z are available on the SDP-H1
product page. The comprehensive ACE user guide is available on the ACE software page.
Figure 1 shows the typical setup of the EVAL-AD7386FMCZ.
Figure 1. EVAL-AD7386FMCZ EVALUATION BOARD (LEFT) CONNECTED TO SDP-H1 BOARD (RIGHT)
The EVAL-AD7386FMCZ is powered by the SDP-H1\\board by default. External power supplies can be applied. See Table 1 for a description of connectors required and Table 2 for the link configuration required. To evaluate the AD7386 with the EVAL-AD7386FMCZ, take the following steps:
Figure 2. Typical Setup of the EVAL-AD7386FMCZ and the SDP-H1 Board
The EVAL-AD7386FMCZ perates from a 12 V power supply. Ensure that all link positions are set according to the required operating mode before applying power and signals to the EVAL-AD7386FMCZ. See Table 2 for the complete list of link options. The EVAL-AD7386FMCZ is powered by the SDP-H1 board by default. External power supplies can also be applied to the board. See Table 1 for a description of the connectors used and Table 2 for the link configurations required. Figure 3 shows the functional block diagram of the EVAL-AD7386FMCZ with the onboard AD7386.
Table 1. Optional External Power Supplies
Power Supply | Connector | Voltage Range | Description |
---|---|---|---|
12V | P4-1 | 12+/- 10% | Mainboard power supply for all internal voltage regulators |
GND | P4-2 | 0 | Ground |
EXT_VCC | P5-1 | 3.3+/- 5% | ADC analog power supply |
GND | P5-2 | 0 | Ground |
EXT_VLOGIC | P5-3 | 2.3+/- 5% | Digital serial peripheral input (SPI) power supply |
EXT_AMP_PWR+ | P6-1 | 5 +/- 5% | Amplifier positive power supply |
EXT_GND | P6-2 | 0 | Ground |
EXT_AMP_PWR- | P6-3 | -2.5 +/- 5% | Amplifier negative power supply |
Figure 3. EVAL-AD7386FMCZ Functional Block Diagram
Multiple link options must be set correctly to select the appropriate operating set up before using the EVAL-AD7386FMCZ. The functions of these options are detailed in Table 2.
Ensure that all link positions are set as required by the selected operating mode before applying power and signals to the EVAL-AD7386FMCZ. Table 2 shows the default positions of the links when the EVAL-AD7386FMCZ is packaged.
Table 2. Link Options for EVAL-AD7386FMCZ
Link Name | Function | Default Position | Description |
---|---|---|---|
LK1 | Internal or external selection for the negative supply of the amplifier | 1 | Use the internal −2.5 V from the onboard ADP7182 for the negative supply of the amplifier via the ADP5600. |
LK2 | Internal or external selection for the positive supply of the amplifier | 1 | Use the internal 5 V from the onboard ADP7104 for the positive supply of the amplifier. |
LK3 | Internal or external selection for the 12 V supply | 1 | Use the 12 V power supply from the SDP-H1 board. Change to Position 3 to use an external supply. |
LK4 | Selection for the external voltage reference (VREF) of the ADC | 3-4 | Use the internal 3.3 V from the ADR4533 for VREF. Change to Position 5 connected to Position 6 (Position 5-6) to use the internal 2.5 V from the ADR4525. |
LK5 | Selection for the logic voltage (VLOGIC) of the ADC | 3-4 | Change to Position 1-2 (link shorted on Pin 1 and Pin 2) to use the external source. Change to Position 3-4 (link shorted on Pin 3 and Pin 4) to use the onboard ADP166. Change to Position 5-6 (link shorted on Pin 5 and Pin 6) to use VLOGIC from the EVAL-SDP-CH1Z. |
JP1, JP2 | Amplifier selection for AINA− | 1(SMD resistor) | Use the onboard ADA4896-2 amplifier for signal conditioning. Change to Position 3 to use an external amplifier mezzanine card (AMC) instead of the onboard ADC driver. |
JP3, JP6 | Amplifier selection for AINA+ | 1(SMD resistor) | Use the onboard ADA4896-2 amplifier for signal conditioning. Change to Position 3 to use an external amplifier mezzanine card (AMC) instead of the onboard ADC driver. |
JP4 | Selection for the VREF of the ADC | 3(SMD resistor) | The REFIO pin is driven with the on-board reference. Change to position to 2 to use an external voltage reference. |
JP5 | Selection for the VCC of the ADC | 1(SMD resistor) | The VCC pin is driven with the on-board reference 3.3V through ADP166. Change to position 3 to use external VCC. |
The sockets and connectors on the EVAL-AD7386FMCZ are described in Table 3. The default interface to the EVAL-AD7386FMCZ is via the 160-way connector, which connects the EVAL-AD7386FMCZ to the SDP-H1 board. When using the EVAL-AD7386FMCZ in standalone mode, communication is achieved via the P3 header pins.
There are several test points and single-in-line (SIL) headers on the EVAL-AD7386FMCZ. These test points and headers provide access to the evaluation board signals to allow probing, evaluation, and debugging.
Table 3. On-Board Sockets and Connectors
Connector | Function |
---|---|
J1 | Analog Input 0 for Channel A |
J2 | Analog Input 1 for Channel A |
J3 | Analog Input 0 for Channel B |
J4 | Analog Input 1 for Channel B |
P1 | Amplifier mezzanine card input |
P2 | Amplifier mezzanine card output |
P3 | Digital SPI signals |
P4 | Main board power supply (12 V) for all internal voltage regulators |
P5 | ADC power supply and digital SPI power supply |
P6 | Amplifier power supply |
P7 | Field-programmable gate array (FPGA), mezzanine card (FMC) to low pin count (LPC), SDP connector |
EXT_REF | External voltage reference |
Download the ACE software from the AD7386 product page and install the ACE software on the PC before using the EVAL-AD7386FMCZ. The installation process consists of the ACE software installation and the SDP-H1 driver installation. To ensure that the evaluation system is recognized when it is connected to the PC, install the ACE software and SDP-H1 driver before connecting the EVAL-AD7386FMCZ and the SDP-H1 board to the USB port of the PC.
To install the ACE software, take the following steps:
Figure 4. ACE Software Installation Confirmation
Figure 5. License Agreement
Figure 6. Choose Installation Location
Figure 7. Choose Components Section
Figure 8. Windows Security Window
Figure 9. Installation in Progress
Figure 10. Installation Completed
Figure 2 shows a diagram of the connections between the EVAL-AD7386FMCZ and the SDP-H1 board. To ensure that the evaluation system is recognized when it is connected to the PC, install the ACE software and SDP-H1 driver before connecting the EVAL-AD7386FMCZ and the SDP-H1 board to the USB port of the PC. When the ACE software installation is complete, set up the EVAL-AD7386FMCZ and the SDP-H1 board as described in the following sections.
To connect the EVAL-AD7386FMCZ and the SDP-H1 board to the PC, take the following steps:
To verify the board connection, take the following steps:
Figure 11. Device Manager Window
Always remove power from the SDP-H1 board and the EVAL-AD7386FMCZ or click the reset tact switch located alongside the USB port before disconnecting the EVAL-AD7386FMCZ from the SDP-H1 board.
When the EVAL-AD7386FMCZ and SDP-H1 boards are properly connected to the PC, launch the ACE software. To launch the ACE software, take the following steps:
Figure 12. ACE Software Main Window
Figure 13. EVAL-AD7386FMCZ View
After completing the steps in the Software Installation Procedures section and the Evaluation Board Setup Procedures section, set up the system for data capture as follows:
See the Software Installation Procedures section and the Evaluation Board Setup Procedures section for additional information.
Figure 14. Chip View
Figure 15. Channel Selection
Figure 16. Pop-Up Configurable Window
Click the AD7386 chip icon in the board view to open the window shown in Figure 14. The chip view shows the configurable block diagram of AD7386.
Click the multiplexer icons circled in red (see Figure 15) to select the ADC channel pairs for conversion (AINA0/AINB0 and AINA1/AINB1).
The AD7386 offers an oversampling function on-chip and has two user-configurable oversampling modes, normal average and rolling average. Click the OSC block to configure the oversampling ratio.
The AD7386 offers an oversampling function on-chip and has two user-configurable oversampling modes, normal average and rolling average. Click the OSC block to configure the oversampling ratio.
The AD7386 offers an option to have a 1-wire or a 2-wire configuration for serial communication. Click the Control Logic block to configure this option.
Configure 2-wire mode by setting the SDO bit in the CONFIGURATION2 register (Address 0x02) to 0. In 2-wire mode, the conversion result for ADC A is output on the SDOA pin, and the conversion result for ADC B is output on the SDOB/ALERT pin.
In applications where slower throughput rates are allowed, or normal average oversampling is used, the serial interface can operate in 1-wire mode. In 1-wire mode, the conversion results from ADC A and ADC B are output on the serial output, SDOA. Additional SCLK cycles are required to propagate all data. ADC A data is output first, followed by ADC B conversion results.
Click Proceed to Memory Map in the bottom right corner of the chip view window to open the window shown in Figure 17. The memory map shows all registers of AD7386.
Figure 17. Memory Map Window
The registers are populated with default values when powered up. To implement the values changed in all the registers, click Apply Changes to write to the registers.
To implement changes on a selected register when the values of a register are changed, click Apply Selected to write the new value on the selected register to the AD7386.
Click Read All to read the values of all the registers from the chip.
Click Read Selected to read the selected register from the chip.
Click Reset Chip to prompt the software to reset the AD7386.
Click Diff to check for differences in register values between the software and the chip.
To revert all the register values to their defaults, click Software Defaults and then Apply Changes to write to the AD7386.
Click Proceed to Analysis in the chip view to open the window shown in Figure 18. The analysis view contains the Waveform tab, Histogram tab, and FFT tab.
Figure 18. Analysis View
The Waveform tab displays data in the form of time vs. discrete data values with the results (see Figure 19). The CAPTURE pane contains capture settings that apply to the registers automati¬cally before data capture.
Figure 19. Waveform Tab
The Sample Count dropdown list allows the user to select the number of samples per channel per capture. The SPI Frequency (MHz) dropdown list allows the user to select the SPI clock frequency used to transfer data between the FPGA device and the AD7386 during device register reads and writes and during data capture. This frequency must be set relatively higher than the set throughput rate. The user can enter the input sample frequency in kSPS in the Sampling Frequency(ksps) box. Refer to the AD7386 datasheet to determine the maximum sampling frequency for the selected mode.
The Over Sampling Ratio box includes options to disable the oversampling ratio function (Disabled) or to set the oversampling ratio between 2 and 32, which, when selected, automatically enables the oversampling ratio function and provides an improved signal to noise ratio (SNR) performance. Refer to the AD7386 datasheet to determine the maximum oversampling ratio for the selected oversampling mode. When an option other than Disabled is selected, a drop-down list appears. Select 18-Bit Resolution to enter 18-bit resolution mode. The resolution boost is used in conjunction with the oversampling rate to provide two extra bits of resolution. The Over Sampling Mode dropdown list allows the user to select the mode of oversampling. This setting is only applicable when oversampling is enabled.
Click Run Once to start a data capture of the samples at the sample rate specified in the Sample Count dropdown list box. These samples are stored on the FPGA device and are transferred to the PC only when the sample frame is complete.
Click Run Continuously to start a data capture that gathers samples continuously with one batch of data at a time. This option runs the Run Once operation continuously.
Display Channels allow the user to select the channels to capture. The channel data is shown only if that channel is selected before the capture.
Waveform Results display amplitude, sample frequency, and noise analysis data for the selected channels.
Click Export to export the captured data. The waveform, histogram, and FFT data are stored in .xml files along with the values of parameters at capture.
The data Waveform graph shows each successive sample of the ADC output. The user can zoom and pan the waveform using the embedded waveform tools. The channels to display can be selected in the Display Channels section.
Click the display units dropdown list to select whether the data graph displays in units of hexadecimal, volts, or codes. The axis controls are dynamic. When selecting either y-scale dynamic or x-scale dynamic, the corresponding axis width automatically adjusts to show the entire range of the ADC results after each batch of samples.
The Histogram tab contains the histogram graph and the results pane, as shown in Figure 20.
The RESULTS pane displays the information related to the dc performance.
The histogram graph displays the number of hits per code within the sampled data. This graph is useful for dc analysis and indicates the noise performance of the device.
Figure 21 shows the FFT tab, which displays fast Fourier transform (FFT) information for the last batch of samples gathered.
Figure 21. FFT Tab
This section sets up the preferred configuration of the FFT analysis, including the number of tones analyzed and whether the fundamental is set manually.
This section sets up the preferred windowing type used in the FFT analysis. The number of harmonic bins and fundamental bins that must be included in the analysis are also set up in this section.
These sections set up the fundamental frequency included in the FFT analysis. Type in the values for the Two-Tone Analysis section when two frequencies are analyzed.
Signal displays the sampling frequency, fundamental frequency, and fundamental power.
Noise displays the SNR and other noise performance results.
Distortion displays the harmonic content of the sampled signal and dc power when viewing the FFT analysis.
To exit the software, click File and Exit.
Board schematic, layout and BOM files.ad7386_eval_board_design_files.zip