Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
resources:eval:user-guides:eval-ad5940:tools:sensorpal_setup_guide [22 May 2019 13:45] Micheál Lamberesources:eval:user-guides:eval-ad5940:tools:sensorpal_setup_guide [10 Mar 2022 06:33] (current) Hans Laurence Josafat
Line 1: Line 1:
 ====== How to setup and use SensorPal ====== ====== How to setup and use SensorPal ======
  
-SensorPal is an easy to use configuration tool designed to program the AD5940 and display measurement results. To download the latest SensorPal installer click on [[ftp://ftp.analog.com/pub/MicroConverter/SensorPal/SensorPal%20Installer_v1013.exe|this link]]+SensorPal is an easy to use configuration tool designed to work with the the **EVAL-AD5940BIOZ, EVAL-AD5940ELCZ, EVAl-AD5941ELCZ** and **EVAL-AD5941BATZ** evaluation kits. It provides an intuitive graphical user interface to facilitate rapid measurement prototyping and results analysis through graph form
  
-SensorPal is designed to work with the the EVAL-AD5940BIOZ and EVAL-AD5940ELCZ evaluation kits.+=====Download Instructions===== 
 +To download the latest SensorPal installer click on the link below. **Note**, if the link do not open correctly, try using an alternative browser such as Google Chrome, Microsoft Edge, etc. 
 +  - AD5940 [[adi>en/products/ad5940.html#product-requirement|SensorPal GUI Installer]] 
 +{{ :resources:eval:user-guides:eval-ad5940:tools:sensorpalinstaller_analog_com.png?600 |}}
  
 =====Installation Instructions===== =====Installation Instructions=====
-  - Navigate to the folder where the installer was downloaded and double click on SensorPal Installer_v1013.exe to launch the executable+  - Navigate to the folder where the installer was downloaded and double click on SensorPal Installer_v2100.exe to launch the executable
   - Follow the Install Wizard instructions to complete the setup.   - Follow the Install Wizard instructions to complete the setup.
   - When complete click Finish   - When complete click Finish
Line 13: Line 16:
   - To launch SensorPal go to the start menu-> All Programs->SensorPal   - To launch SensorPal go to the start menu-> All Programs->SensorPal
   - To get started ensure the AD5940 evaluation kit is connected to the PC. Click on the Firmware Load button in the top toolbar as per below screenshot. {{ :resources:eval:user-guides:eval-ad5940:tools:firmware_load.png?nolink&600 |}}   - To get started ensure the AD5940 evaluation kit is connected to the PC. Click on the Firmware Load button in the top toolbar as per below screenshot. {{ :resources:eval:user-guides:eval-ad5940:tools:firmware_load.png?nolink&600 |}}
-  - Select the correct board. It is should be DAPLINK(E:\) then click Update Firmware {{ :resources:eval:user-guides:eval-ad5940:tools:firmware_load_2.png?nolink&600 |}}+  - Select the correct board, it should be similar to DAPLINK(E:\). Then click Update Firmware {{ :resources:eval:user-guides:eval-ad5940:tools:firmware_load_2.png?nolink&600 |}}
   - Once the firmware is loaded plug out the evaluation kit from the PC and reconnect to power cycle the hardware.   - Once the firmware is loaded plug out the evaluation kit from the PC and reconnect to power cycle the hardware.
-  - In the middle of the screen hit the refresh symbol beside the Com port dropdown. Then select the com port the ADICUP3029 microcontroller is connected to from the drop down list. {{ :resources:eval:user-guides:eval-ad5940:tools:comm_port.png?nolink&600 |}}+  - In the center of the screen hit the refresh symbol beside the Com port drop-down text box. Then select the com port the ADICUP3029 microcontroller is connected to from the drop down list. {{ :resources:eval:user-guides:eval-ad5940:tools:comm_port.png?nolink&600 |}}
   - To select an application to run, drag it from the left hand column of techniques and drop into the Work Area. A number of configurable parameters are available. Modify them as required.   - To select an application to run, drag it from the left hand column of techniques and drop into the Work Area. A number of configurable parameters are available. Modify them as required.
   - To begin a measurement click on the green Measure button to the right side of the GUI.   - To begin a measurement click on the green Measure button to the right side of the GUI.
   - The measurement results will be displayed in the graph window.   - The measurement results will be displayed in the graph window.
   - To stop a measurement click on the Abort Measurement button.   - To stop a measurement click on the Abort Measurement button.
resources/eval/user-guides/eval-ad5940/tools/sensorpal_setup_guide.1558525532.txt.gz · Last modified: 22 May 2019 13:45 by Micheál Lambe