Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
resources:eval:user-guides:eval-ad5940:software_examples:ad5940_ramp [08 Jul 2019 17:28]
Micheál Lambe
resources:eval:user-guides:eval-ad5940:software_examples:ad5940_ramp [22 Oct 2019 17:03]
Micheál Lambe
Line 29: Line 29:
   - Set S5 to Wall/USB to power the board from the USB cable{{ :​resources:​eval:​user-guides:​eval-adicup3029:​reference_designs:​img_20170612_144023_hdr.jpg?​800 |}}   - Set S5 to Wall/USB to power the board from the USB cable{{ :​resources:​eval:​user-guides:​eval-adicup3029:​reference_designs:​img_20170612_144023_hdr.jpg?​800 |}}
   - Place the **EVAL-AD5940ELCZ** on top of the **EVAL-ADICUP3029**.   - Place the **EVAL-AD5940ELCZ** on top of the **EVAL-ADICUP3029**.
-  - Ensure jumper on JP10 and JP11 is on PIN2 and PIN4 (to use the USB connected probe with EVAL-AD5940ELCZ,​ JP9,JP10 and JP11 should be configured to position C - pins 5 and 6) +  - Ensure jumper on JP10 and JP11 is on PIN2 and PIN4 to connect the dummy sensor to the AD5940 ​(to use the USB connected probe with EVAL-AD5940ELCZ,​ JP9,JP10 and JP11 should be configured to position C - pins 5 and 6) 
-  - Place jumper in position B on JP6 to connect the 1kΩ||3kΩ RE0 and SE0+  - Place jumper in position B on JP6 to connect the 10kΩ||10kΩ resistor divider between ​RE0 and SE0
   - Plug in the micro USB cable into the (P10) USB port on the EVAL-ADICUP3029,​ and the other end into the PC or laptop.   - Plug in the micro USB cable into the (P10) USB port on the EVAL-ADICUP3029,​ and the other end into the PC or laptop.
  
resources/eval/user-guides/eval-ad5940/software_examples/ad5940_ramp.txt · Last modified: 22 Oct 2019 17:03 by Micheál Lambe