This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:eval-ad5940:software_examples:ad5940_bia [30 Nov 2018 13:09] – [Configuring the Software] Micheál Lambe | resources:eval:user-guides:eval-ad5940:software_examples:ad5940_bia [05 Dec 2019 19:00] (current) – Gustavo Velasco-Hernández | ||
---|---|---|---|
Line 16: | Line 16: | ||
* EVAL-AD5940BIOZ | * EVAL-AD5940BIOZ | ||
* Z-Test Board | * Z-Test Board | ||
- | * Mirco USB to USB cable | + | * Micro USB to USB cable |
* PC or Laptop with a USB port | * PC or Laptop with a USB port | ||
* Custom Cables (Optional) | * Custom Cables (Optional) | ||
Line 30: | Line 30: | ||
- Set S5 to Wall/USB to power the board from the USB cable{{ : | - Set S5 to Wall/USB to power the board from the USB cable{{ : | ||
- Place the **EVAL-AD5940BIOZ** on top of the **EVAL-ADICUP3029**.{{ : | - Place the **EVAL-AD5940BIOZ** on top of the **EVAL-ADICUP3029**.{{ : | ||
+ | - Connect the AD5940 Z Test board to the EVAL-AD5940BIOZ board | ||
- All jumpers should be in their default position | - All jumpers should be in their default position | ||
- Plug in the micro USB cable into the (P10) USB port on the EVAL-ADICUP3029, | - Plug in the micro USB cable into the (P10) USB port on the EVAL-ADICUP3029, | ||
+ | ==== AD5940 Z Test Board ==== | ||
+ | |||
+ | The AD5940 Z Test board is designed to model skin impedance, body impedance, electrode contact impedance and electrode impedance. There are 5 banks of switches on the board labelled S1, S2, S3, S4 and S5. The function of each bank is described in the following table: | ||
+ | ^ Switch Bank ^ Bank Function ^ | ||
+ | | S1 | Used to model Body Impedance | ||
+ | | S2 | Used to model contact impedance on F+ electrode | | ||
+ | | S3 | Used to model contact impedance on S+ electrode | | ||
+ | | S4 | Used to model contact impedance on F- electrode | | ||
+ | | S5 | Used to model contact impedance on S- electrode | | ||
+ | |||
+ | The following tables indicate the resistor or capacitor value associated with each switch in the bank. Moving the switch to the ON position connects the corresponding resistor or capacitor value in series on the signal path. If more than one switch is active the corresponding resistor values are connected in series. | ||
+ | <WRAP column 30%> | ||
+ | ^ S1 Bank ^ Corresponding Res/Cap Value ^ | ||
+ | | S1 | 100 Ω | | ||
+ | | S2 | 200 Ω | | ||
+ | | S3 | 300 Ω | | ||
+ | | S4 | 340 Ω | | ||
+ | | S5 | 510 Ω | | ||
+ | | S6 | 1 kΩ | | ||
+ | | S7 | 2 kΩ | | ||
+ | | S8 | 3.01 kΩ | | ||
+ | | S9 | 4.02 kΩ | | ||
+ | | S10 | 4.99 kΩ | | ||
+ | | S11 | 1000 pF | | ||
+ | | S12 | 0.01 μF | | ||
+ | </ | ||
+ | <WRAP column 30%> | ||
+ | ^ S2 Bank ^ Corresponding Res/Cap Value ^ | ||
+ | | S1 | 100 Ω | | ||
+ | | S2 | 200 Ω | | ||
+ | | S3 | 300 Ω | | ||
+ | | S4 | 402 Ω | | ||
+ | | S5 | 10 kΩ | | ||
+ | | S6 | 23.7 kΩ | | ||
+ | | S7 | 42.2 kΩ | | ||
+ | | S8 | 42.2 kΩ | | ||
+ | | S9 | 100 kΩ | | ||
+ | | S10 | 200 kΩ | | ||
+ | | S11 | 1000 pF | | ||
+ | | S12 | 0.01 μF | | ||
+ | </ | ||
+ | <WRAP column 30%> | ||
+ | ^ S3 Bank ^ Corresponding Res/Cap Value ^ | ||
+ | | S1 | 100 Ω | | ||
+ | | S2 | 200 Ω | | ||
+ | | S3 | 300 Ω | | ||
+ | | S4 | 402 Ω | | ||
+ | | S5 | 4.22 MΩ | | ||
+ | | S6 | 4.22 MΩ | | ||
+ | | S7 | 1.43 MΩ | | ||
+ | | S8 | 1 MΩ | | ||
+ | | S9 | 300 kΩ | | ||
+ | | S10 | 300 kΩ | | ||
+ | | S11 | 1000 pF | | ||
+ | | S12 | 0.01 μF | | ||
+ | </ | ||
+ | <WRAP clear></ | ||
+ | <WRAP column 30%> | ||
+ | ^ S4 Bank ^ Corresponding Res/Cap Value ^ | ||
+ | | S1 | 100 Ω | | ||
+ | | S2 | 200 Ω | | ||
+ | | S3 | 300 Ω | | ||
+ | | S4 | 402 Ω | | ||
+ | | S5 | 499 Ω | | ||
+ | | S6 | 1 kΩ | | ||
+ | | S7 | 2 kΩ | | ||
+ | | S8 | 3.01 kΩ | | ||
+ | | S9 | 4.02 kΩ | | ||
+ | | S10 | 4.99 kΩ | | ||
+ | | S11 | 1000 pF | | ||
+ | | S12 | 0.01 μF | | ||
+ | </ | ||
+ | <WRAP column 30%> | ||
+ | ^ S5 Bank ^ Corresponding Res/Cap Value ^ | ||
+ | | S1 | 100 Ω | | ||
+ | | S2 | 200 Ω | | ||
+ | | S3 | 300 Ω | | ||
+ | | S4 | 402 Ω | | ||
+ | | S5 | 499 Ω | | ||
+ | | S6 | 1 kΩ | | ||
+ | | S7 | 2 kΩ | | ||
+ | | S8 | 3.01 kΩ | | ||
+ | | S9 | 4.02 kΩ | | ||
+ | | S10 | 4.99 kΩ | | ||
+ | | S11 | 1000 pF | | ||
+ | | S12 | 0.01 μF | | ||
+ | </ | ||
+ | <WRAP clear></ | ||
+ | |||
+ | ===== AD5940 Z Test Schematic and Layout ===== | ||
+ | |||
+ | <WRAP round 80% download> | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | {{ : | ||
+ | </ | ||
===== Obtaining the Source Code ===== | ===== Obtaining the Source Code ===== | ||
Line 38: | Line 136: | ||
<WRAP round 80% download> | <WRAP round 80% download> | ||
- | Add link to Git | + | [[https:// |
- | + | ||
</ | </ | ||