Help and Support
Do you need help or have general support questions? This page will help you resolve these.
This page has a quickstart troubleshooting approach that goes over some very general questions and common pitfalls, but if you have a specific issue which requires more information or detail please contact us through EngineerZone or Email. (links can be found further down on the page where to direct specific questions)
What to do When Things Go Wrong
There are many things that can go wrong with an ecosystem this complex, but if you are having issues getting the board or software working, here are a few simple things you can try before contacting Analog Devices.
Check the Power on ADICUP3029
Check the Power on EVAL-AD5940xxxx
Program the ADuCM3029
Sometimes a flashed program doesn't run properly or can make it difficult to run the debugger.
The first thing to try in this case, is to
drag and drop a known good .HEX or .BIN program into flash.(something with quick visible indicators works best)
If drag and drop is not working, it may be necessary to erase the flash. To do so:
-
Make sure that the
USB is selected on the three way
UART switch (S2).
Power cycle the ADICUP3029 board while holding down the boot switch (S3)
Select the mbed serial COM port in the CrossCore Serial Flash Programmer, and erase the flash.
-
If the mass erase didn't work, and you are trying to drag and drop a large .BIN file on EVAL-ADICUP3029 Rev B hardware, it's possible that the mbed interface file needs to be updated to support your application.
-
Once you are in “maintenance mode” you should drag and drop the latest interface file onto your maintenance drive. That file can be downloaded at the bottom of
Maintenance Drive Page.
Not receiving/transmitting data to the
UART
Make sure that the
UART switch (S2) is positioned in the correct destination to transmit/receive
UART data.
I'
m trying to program/debug, but I'
m getting errors.
Check the drives attached to your computer, do you see a mass storage device called
DAPLINK or
Maintenance? If you see the Maintenance drive and your
USB is plugged in, then likely the ADuCM3029 isn't being powered, which means the power switch (S5) is likely in the “BATT” position. Flip it “WALL/
USB” and unplug/reconnect your
USB cable to your computer, and try to programming again.
This is just a brief self-help guide to troubleshooting common issues. If you have other questions that need answering please direct those requests to the locations outlined below.
Hardware, Software, and Documentation Questions
If you have any questions regarding the ADICUP3029 base board or are experiencing any problems using the AD5940 SDK or issues following any of the documentation feel free to ask us a question.
-
ADICUP3029 hardware
ADuCM3029 silicon
ADICUP3029 documentation
-
AD5940 silicon
AD5940 documentation
AD5940 evaluation boards
When asking a question please take the time to give a detailed description of your problem. If you are experiencing a problem please state the steps you have executed, the result you expected you would get and the result you actually got. By doing so you enable us to provide you precise and detailed answers in a timely manner.
Before asking questions please take the time to check if somebody else already asked the same question. You might just find your question already answered.
End of Document