Wiki

The most recent version of this page is a draft.DiffThis version (13 Jan 2021 15:01) was approved by Mohriz Hassan.

This is an old revision of the document!


Power Connections

There are two options for supplying power to the board. The default power supply comes from the connector P2 5V pin provided by the host microcontroller. This supply drives the ADP5320 to generate low noise 5V, 1.8V and 1.2 V and 3.3V supplies for the ADAS1021. Ensure that P9 and P10 are in position 2,3 with AVDDS5V,1V8, IOVDD and DVDD jumpers in place. Alternatively, the board can be powered from connector P1 and P7. • Remove AVDD5V, 1V8, IOVDD and DVDD jumpers • Supply power through P1 and P7.

/srv/wiki.analog.com/data/pages/resources/eval/user-guides/eval-ad5940/hardware/power_connections.txt · Last modified: 15 Jan 2021 13:52 by Mohriz Hassan