Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
resources:eval:user-guides:eval-ad5940:hardware:eval-ad5940elcz [10 Aug 2021 12:01]
Akila M [Connectors and Jumpers]
resources:eval:user-guides:eval-ad5940:hardware:eval-ad5940elcz [10 Aug 2021 12:01] (current)
Akila M [EC Gas Connector]
Line 62: Line 62:
 Note, the USB to crocodile cable is intended for rapid prototyping. There is a parasitic resistance and capacitance associated with it which may effect measurement accuracy. This is especially through for high frequency impedance measurements. Note, the USB to crocodile cable is intended for rapid prototyping. There is a parasitic resistance and capacitance associated with it which may effect measurement accuracy. This is especially through for high frequency impedance measurements.
 ===== EC Gas Connector ===== ===== EC Gas Connector =====
-M1 is an Electrochemical gas sensor socket. Standard EC gas sensors can be connected to perform gas sensor measurements. When measuring a Gas sensor ensure JP9, JP10 and JP11 are switched to position ​B,and A respectively.+M1 is an Electrochemical gas sensor socket. Standard EC gas sensors can be connected to perform gas sensor measurements. When measuring a Gas sensor ensure JP9, JP10 and JP11 are switched to position A.
 ===== BNC Connector ===== ===== BNC Connector =====
 The BNC connector is connected to the AD5940 via LTC6078 amplifier. This amplifier can be used with high impedance sensor'​s such as pH sensors and for water conductivity measurements. The BNC connector is connected to the AD5940 via LTC6078 amplifier. This amplifier can be used with high impedance sensor'​s such as pH sensors and for water conductivity measurements.
resources/eval/user-guides/eval-ad5940/hardware/eval-ad5940elcz.txt · Last modified: 10 Aug 2021 12:01 by Akila M