This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:eval-ad5940:hardware:eval-ad5940bioz [28 Nov 2018 13:35] – Updated Micheál Lambe | resources:eval:user-guides:eval-ad5940:hardware:eval-ad5940bioz [13 Feb 2024 11:02] (current) – [USB Connector] Akila M | ||
---|---|---|---|
Line 7: | Line 7: | ||
* Body Impedance Analysis (2-wire) (BIOZ-2Wire) | * Body Impedance Analysis (2-wire) (BIOZ-2Wire) | ||
The platform is an Arduino UNO form factorbase board. This section describes the key features of the board and how to set it up to take measurements. | The platform is an Arduino UNO form factorbase board. This section describes the key features of the board and how to set it up to take measurements. | ||
+ | {{ : | ||
+ | {{ : | ||
===== Connectors and Jumpers ===== | ===== Connectors and Jumpers ===== | ||
All the connectors and their default configurations are described in the table below. | All the connectors and their default configurations are described in the table below. | ||
Line 25: | Line 26: | ||
^ P15 (LDO Aux Enable) | 1-2| LDO Enabled | ^ P15 (LDO Aux Enable) | 1-2| LDO Enabled | ||
| ::: | 2-3| LDO Disabled (Default) | | ::: | 2-3| LDO Disabled (Default) | ||
- | ^ JP6 (SMD Jumper) | A| Pull up resistor connected to electrode bias | + | ^ JP5 (Default DNI) | A| Pull up resistor |
- | | ::: | B| Pull down resistor connected electrode bias | | + | | ::: | B| Pull down resistor |
- | ^ JP9 (DE0 Mux) | + | ^ JP6 |
- | | ::: | B| DE0 connected | + | | ::: | B| Pull down resistor (R42)connected |
- | | ::: | C| DE0 connected to USB port | | + | ^ JP7 (Bias Select) | 3-1| Electrode bias connected to REFOUTS |
- | ^ JP10 (RE0 Mux) | A| RE0 connected to dummy network | | + | | ::: |
- | | ::: | + | | ::: |
- | | ::: | + | ^ JP8 | A| Connected. EEPROM write protect | |
- | ^ JP11 (SE0 Mux) | A| SE0 connected to dummy network | | + | ^ P16 |
- | | ::: | B| SE0 connected | + | | ::: |
- | | ::: | + | ^ P17 |
- | ^ JP4 (Cable Shield Mux)| A| Shield connected | + | | ::: |
- | | ::: | B| Shield connected to Bead | | + | |
- | ^ JP5 | + | |
- | | ::: | + | |
- | | ::: | C| Connected | + | |
===== USB Connector ===== | ===== USB Connector ===== | ||
+ | The Micro USB connector, P6, on the EVAL-AD5940BIOZ board serves 2 functions. | ||
+ | * The provided ECG cables can be connected to a human body simulator which can be used to verify ECG, body composition etc. Note: The EVAL-AD5940BIOZ must never be connected to the human body while the board is connected to a PC or Laptop | ||
+ | * The provided AD5940 Z Test board can also be connected to the Micro USB connecter. This board contains a number of banks of resistors and capacitors which can be used to model Body Impedance, Skin Impedance, Electrode impedances and Contact impedance. These resistor values are configured with the various switches. | ||
+ | Note, P6 USB connector must only be used with the supplied AD5940 Z Test board or the provided ECG Cables. No other cable should ever be connected. | ||
+ | |||
+ | Micro USB pinout for connecting ECG Cables: | ||
+ | ^USB pin | ||
+ | ^1 | ||
+ | ^2 |S+ (ECG IN+)| N/C| | ||
+ | ^3 | ||
+ | ^4 | N/C |N/C | | ||
+ | ^5 | ||
+ | |||
+ | |||
+ | ===== Schematics, PCB Layout, Bill of Materials ===== | ||
+ | <WRAP round 80% download> | ||
+ | |||
+ | EVAL-AD5940BIOZ Rev B Design Files | ||
+ | * {{ : | ||
+ | * {{ : | ||
+ | * {{ : | ||
+ | * {{ : | ||
+ | |||
+ | </ | ||
+ | |||