This is an old revision of the document!
The EVAL-AD5940BIOZ shield was designed specifically for carrying out bio-electric measurements. These include:
The platform is an Arduino UNO form factorbase board. This section describes the key features of the board and how to set it up to take measurements.
All the connectors and their default configurations are described in the table below.
Connector | Jmpr Position. | Description |
---|---|---|
JP1 (DVDD) | A | DVDD powered from 3.3V on Arduino Header (Default) |
B | DVDD powered from LDO | |
C | DVDD powered from external source connected to P11 | |
JP2 (AVDD) | A | AVDD powered from 3.3V on Arduino Header (Default) |
B | AVDD powered from LDO | |
C | AVDD powered from external source connected to P8 | |
JP3 (Reset) | A | Reset pin connected to ARST Button (Default) |
B | Reset pin connected to Arduino Header Reset pin | |
C | Reset pin connected to Arduino header P1.3 (Default) | |
P9 (LDO Enable) | 1-2 | LDO Enabled |
2-3 | LDO Disabled (Default) | |
P15 (LDO Aux Enable) | 1-2 | LDO Enabled |
2-3 | LDO Disabled (Default) | |
JP6 (SMD Jumper) | A | Pull up resistor connected to electrode bias |
B | Pull down resistor connected electrode bias | |
JP9 (DE0 Mux) | A | DE0 connected to Gas sensor connector |
B | DE0 connected to dummy network | |
C | DE0 connected to USB port | |
JP10 (RE0 Mux) | A | RE0 connected to dummy network |
B | RE0 connected to gas sensor | |
C | RE0 connected to USB port | |
JP11 (SE0 Mux) | A | SE0 connected to dummy network |
B | SE0 connected to gas sensor | |
C | SE0 connected to USB port | |
JP4 (Cable Shield Mux) | A | Shield connected to CE0 |
B | Shield connected to Bead | |
JP5 (BNC Mux) | A | Water conductivity |
B | pH Measurement | |
C | Connected to AFE1 |