Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
resources:eval:user-guides:eval-ad5940:hardware:eval-ad5940bioz [11 Apr 2019 19:49]
Micheál Lambe [Connectors and Jumpers]
resources:eval:user-guides:eval-ad5940:hardware:eval-ad5940bioz [09 Aug 2021 13:43]
Akila M [USB Connector]
Line 43: Line 43:
   * The provided AD5940 Z Test board can also be connected to the Micro USB connecter. This board contains a number of banks of resistors and capacitors which can be used to model Body Impedance, Skin Impedance, Electrode impedances and Contact impedance. These resistor values are configured with the various switches.   * The provided AD5940 Z Test board can also be connected to the Micro USB connecter. This board contains a number of banks of resistors and capacitors which can be used to model Body Impedance, Skin Impedance, Electrode impedances and Contact impedance. These resistor values are configured with the various switches.
 Note, P6 USB connector must only be used with the supplied AD5940 Z Test board or the provided ECG Cables. No other cable should ever be connected. Note, P6 USB connector must only be used with the supplied AD5940 Z Test board or the provided ECG Cables. No other cable should ever be connected.
 +
 +ECG Cables:
 +Red = F+
 +Black = F-
 +Green = S+
 +Blue = S-
 +
  
 ===== Schematics, PCB Layout, Bill of Materials ===== ===== Schematics, PCB Layout, Bill of Materials =====
resources/eval/user-guides/eval-ad5940/hardware/eval-ad5940bioz.txt · Last modified: 09 Aug 2021 13:43 by Akila M