Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Next revision
Previous revision
Next revision Both sides next revision
resources:eval:user-guides:eval-ad5940:hardware:eval-ad5940bioz [26 Feb 2019 17:49]
Micheál Lambe [Schematics, PCB Layout, Bill of Materials]
resources:eval:user-guides:eval-ad5940:hardware:eval-ad5940bioz [11 Apr 2019 15:44]
Micheál Lambe Updated
Line 43: Line 43:
   * The provided ECG cables can be connected to a human body simulator which can be used to verify ECG, body composition etc. Note: The EVAL-AD5940BIOZ must never be connected to the human body while the board is connected to a PC or Laptop   * The provided ECG cables can be connected to a human body simulator which can be used to verify ECG, body composition etc. Note: The EVAL-AD5940BIOZ must never be connected to the human body while the board is connected to a PC or Laptop
   * The provided AD5940 Z Test board can also be connected to the Micro USB connecter. This board contains a number of banks of resistors and capacitors which can be used to model Body Impedance, Skin Impedance, Electrode impedances and Contact impedance. These resistor values are configured with the various switches.   * The provided AD5940 Z Test board can also be connected to the Micro USB connecter. This board contains a number of banks of resistors and capacitors which can be used to model Body Impedance, Skin Impedance, Electrode impedances and Contact impedance. These resistor values are configured with the various switches.
-Note, the USB connector must only be used with the supplied AD5940 Z Test board or the provided ECG Cables. No other cable should ever be connected.+Note, P6 USB connector must only be used with the supplied AD5940 Z Test board or the provided ECG Cables. No other cable should ever be connected.
  
 ===== Schematics, PCB Layout, Bill of Materials ===== ===== Schematics, PCB Layout, Bill of Materials =====
 <WRAP round 80% download>​ <WRAP round 80% download>​
  
-EVAL-AD5940BIOZ Rev B Schematic+EVAL-AD5940BIOZ Rev B Design Files
   * {{ :​resources:​eval:​user-guides:​eval-ad5940:​hardware:​02_049988b_top.pdf | Schematics}} (PDF)   * {{ :​resources:​eval:​user-guides:​eval-ad5940:​hardware:​02_049988b_top.pdf | Schematics}} (PDF)
 +  * {{ :​resources:​eval:​user-guides:​eval-ad5940:​hardware:​08-049988-01-b.pdf | PCB Layout (PDF)}}
 +  * {{ :​resources:​eval:​user-guides:​eval-ad5940:​hardware:​eval-ad5940bioz_bom.xlsx | Bill of Materials (Excel)}}
 +  * {{ :​resources:​eval:​user-guides:​eval-ad5940:​hardware:​eval-ad5940bioz_fabrication.zip |Fabrication Files (zip)}}
  
 </​WRAP>​ </​WRAP>​
resources/eval/user-guides/eval-ad5940/hardware/eval-ad5940bioz.txt · Last modified: 09 Aug 2021 13:43 by Akila M