This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Last revisionBoth sides next revision | ||
resources:eval:user-guides:ev-mte-agile-900z [17 Sep 2019 10:32] – [Functional block diagram] Added caption for Figure 1 Aditya S | resources:eval:user-guides:ev-mte-agile-900z [17 Sep 2019 11:25] – Added all images and image-captions Aditya S | ||
---|---|---|---|
Line 21: | Line 21: | ||
The EV-MTE-AGILE-900Z evaluation board consists of a module portion, the EV-MOD-AGILE-900Z evaluation board, with an MCU processor and radio. There is also a breakoff portion provided that helps in flashing the MCU and provides multiple options to power up the board. | The EV-MTE-AGILE-900Z evaluation board consists of a module portion, the EV-MOD-AGILE-900Z evaluation board, with an MCU processor and radio. There is also a breakoff portion provided that helps in flashing the MCU and provides multiple options to power up the board. | ||
- | Fig 2,3 | + | {{: |
+ | |||
+ | Figure.2 Front Side of the EV-MTE-AGILE-900Z Board | ||
+ | |||
+ | {{: | ||
+ | |||
+ | Figure.3 Back Side of the EV-MTE-AGILE-900Z Board | ||
==== EVALUATION BOARD COMPONENTS ==== | ==== EVALUATION BOARD COMPONENTS ==== | ||
- | Fig 4 | + | {{: |
+ | |||
+ | Figure.4 EV-MTE-AGILE-900Z Evaluation Board Components | ||
==== POWER SUPPLY OPTIONS ==== | ==== POWER SUPPLY OPTIONS ==== | ||
Line 34: | Line 42: | ||
Table 1 | Table 1 | ||
- | Fig 5 | + | |
+ | {{: | ||
+ | |||
+ | Figure | ||
==== LEDs ==== | ==== LEDs ==== | ||
Line 70: | Line 81: | ||
To route the RF signal to the castellations, | To route the RF signal to the castellations, | ||
- | Fig 6,7,8 | + | {{: |
+ | |||
+ | Figure.6 Switch Positions and RF Castellations | ||
+ | |||
+ | {{: | ||
+ | |||
+ | Figure.7 Capacitor Connection to Route RF Signal to the MMCX Connector | ||
+ | |||
+ | {{: | ||
+ | |||
+ | Figure.8 Capacitor Connection to Route RF Signal to Castellations | ||
==== PINOUT OF THE MODULE ==== | ==== PINOUT OF THE MODULE ==== | ||
Line 76: | Line 97: | ||
EV-MOD-AGILE-900Z board (see Figure 9), a total of 51 pins are accessible through castellations to allow the user to develop a wide variety of applications using the EV-MTE-AGILE-900Z evaluation board. | EV-MOD-AGILE-900Z board (see Figure 9), a total of 51 pins are accessible through castellations to allow the user to develop a wide variety of applications using the EV-MTE-AGILE-900Z evaluation board. | ||
- | Fig 9 | + | {{: |
+ | |||
+ | Figure.9 EV-MOD-AGILE-900Z Evaluation Board | ||
The pinout of the EV-MOD-AGILE-900Z evaluation board is shown in Figure 10. | The pinout of the EV-MOD-AGILE-900Z evaluation board is shown in Figure 10. | ||
- | Fig 10 | + | {{: |
+ | |||
+ | Figure.10 EV-MOD-AGILE-900Z Pinout | ||
Table 5 provides more information about the pins that are accessible through castellations. | Table 5 provides more information about the pins that are accessible through castellations. | ||
Line 107: | Line 132: | ||
- After resetting the board, reinstall the JH6 jumper (removed in Step 3) to flash the EV-COG-AGILE-900Z board at any later point. | - After resetting the board, reinstall the JH6 jumper (removed in Step 3) to flash the EV-COG-AGILE-900Z board at any later point. | ||
- | Fig 11,12,13 | + | {{: |
+ | Figure.11 DAPLINK Drive | ||
+ | {{: | ||
+ | Figure.12 Drag and Drop Procedure Window | ||
+ | {{: | ||
+ | Figure.13 Connecting the EV-MTE-AGILE-900Z Evaluation Board to the EV-COG-AGILE-900Z Evaluation Board | ||