Wiki

This version is outdated by a newer approved version.DiffThis version (18 Sep 2019 14:01) was approved by Aditya S.The Previously approved version (16 Sep 2019 14:02) is available.Diff

This is an old revision of the document!


ev-mote-agile-900z

Description

The EV-MOTE-AGILE-900Z is the secondary kit to demo the AgileNet-6T networking solution. This kit only provides additional nodes and is a supplementary kit to the EV-KIT-AGILE-900Z (Primary kit). This evaluation kit contains the following hardware and equipment:

  • 10 EV-MTE-AGILE-900Z evaluation boards.
  • 10 antenna pigtails.
  • 10 antennas.
  • 10 Li batteries, 3.6 V AA size.

Additional resources

resources/eval/user-guides/ev-mote-agile-900z.1568808067.txt.gz · Last modified: 18 Sep 2019 14:01 by Aditya S