Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
resources:eval:user-guides:ev-gear-expander1z [02 May 2018 19:04] – [COG connectors] Rajalakshmi Jayaramanresources:eval:user-guides:ev-gear-expander1z [28 Jan 2021 17:36] (current) – Fixed bad link for digikey Ioana Chelaru
Line 43: Line 43:
 =====Gear connectors===== =====Gear connectors=====
 The connectors D1 and D2 can be used to connect a Gear. Gear is an addon application board which can be a custom build to serve the required application.  The connectors D1 and D2 can be used to connect a Gear. Gear is an addon application board which can be a custom build to serve the required application. 
-<note important>The gear must have the connector ([[https://www.digikey.com/product-detail/en/hirose-electric-co-ltd/DF17(4.0)-60DP-0.5V(57)/H11146CT-ND/1036112|DF17(4.0)-60DP-0.5V(57)]]) to interface with D1 and D2 connectors.</note> The pinout details for D1 and D2 are same as that of COG connectors ( C1, C2 [[resources:eval:user-guides:ev-cog-ad3029lz:cog_hw_userguide|expander connector section in EV-COG-AD3029LZ wiki]]).+<note important>The gear must have the connector ([[digikey>DF17(4.0)-60DP-0.5V(57)|DF17(4.0)-60DP-0.5V(57)]]) to interface with D1 and D2 connectors.</note> The pinout details for D1 and D2 are same as that of COG connectors ( C1, C2 [[resources:eval:user-guides:ev-cog-ad3029lz:cog_hw_userguide|expander connector section in EV-COG-AD3029LZ wiki]]).
 =====Arduino Uno headers===== =====Arduino Uno headers=====
 The headers A1, A2, A3, A4 and A5 support the shields that are Arduino Uno compatible. The following table captures the signals connected to the headers The headers A1, A2, A3, A4 and A5 support the shields that are Arduino Uno compatible. The following table captures the signals connected to the headers
resources/eval/user-guides/ev-gear-expander1z.txt · Last modified: 28 Jan 2021 17:36 by Ioana Chelaru