Wiki

This version is outdated by a newer approved version.DiffThis version (26 Sep 2018 18:13) was approved by Rajalakshmi Jayaraman, Sreeharsha Srinivas.The Previously approved version (26 Sep 2018 18:12) is available.Diff

This is an old revision of the document!


EV-COG-SMARTMESH1Z

Introduction

EV-COG-SMARTMESH1Z combines reliability and ultra low-power with a native Internet Protocol (IP) layer for a robust, standards-based offering perfect for a broad range of applications. It provides robust wire-free connectivity for applications where low power, reliability, and ease of deployment matter. EV-COG-SMARTMESH1Z is configured in the slave mode and is driven by an external micro-controller.The communication between the controller and EV-COG-SMARTMESH1Z takes place via UART.

The features of SmartMesh IP enabled by EV-COG-SMARTMESH1Z are as follows:-

  • Programming the device using an external micro-controller via Flash SPI lines
  • Flow control for UART communication
  • Obtaining network time for accurate time stamping
  • Switching between CLI and API modes of operation
  • Programming and debugging via J-link
  • Radio silence for radio free sensor data acquisition

This user guide describes the connector pin out,and jumper settings available on board.

The hardware details covers the wire connections between the EV-COG-SMARTMESH1Z and EV-COG-AD3029LZ along with useful links that provides more details pertaining to EV-COG-AD3029LZ and EV-COG-SMARTMESH1Z.

Hardware details

Board image

Primary-side

Secondary-side

The board consists of

  • 32 pin Hirose connector (P1)
  • UART mode switch (SW1)
  • Tag connect point (TC1)
  • Antenna terminal (J4)
  • Flow control jumpers(JP1, JP2, JP3)

32 pin Hirose connector

The Hirose connector P1 interfaces the EV-COG-SMARTMESH1Z board with the MCU Cog. The connector carries VDD, UART, Flash SPI lines and GPIO signals from MCU cog board. The pinout details are given in the following table

Hirose connector (P1) pin numberpin nameMCU Cog signal name
1VSUPPYVDD_RF
2VSUPPYVDD_RF
3GNDGND
4GNDGND
5UART_RX_MCUMCU/UART0_RX
6JMP_TX_RTSNRF_INT
7UART_TX_MCUMCU/UART0_TX
8RADIO_INHIBITMCU/SPI2_CS3
9GNDGND
10IPCS_MISOMCU/SPI2_MISO
11N.CRF_SYS_WAKE
12IPCS_MOSIMCU/SPI2_MOSI
13FLASH_P_ENnMCU/GPIO08
14IPCS_SCKMCU/SPI2_CLK
15N.CP.D [GND, 100K]
16GNDGND
17SLEEPnP.U [VDD_RF, 100K]
18JMP_TX_CTSNSPI2_RDY
19N.C.N.C
20N.CSS_TO_RF
21TIMEnGPIO27
22RESETnGPIO_RF_RESET
23N.CC2/54
24N.CC2/55
25N.CC2/58
26N.C.RF_SYS_WAKE
27N.CC2/59
28IPCS_SSnSPI2_CS0
29GNDGND
30GNDGND
31VSUPPYVDD_RF
32VSUPPYVDD_RF
The following figure shows EV-COG-SMARTMESH1Z connected to EV-COG-AD3029LZ

Schematics, PCB layout, Bill of materials

EV-COG-SMARTMESH1Z Rev A Design and Integration Files

Example Software

Click Here to visit the example software page, and to download the source code from Analog Devices Git repository

Help and support

For help and support on the EV-COG-SMARTMESH1Z use the following SmartMesh-IP_support_link and for the EV-COG-AD3029LZ use EV-COG-AD3029_support_link.

For more information contact us at EngineerZone or Email

resources/eval/user-guides/ev-cog-smartmesh1z.1537978389.txt.gz · Last modified: 26 Sep 2018 18:13 by Rajalakshmi Jayaraman