Wiki

This version is outdated by a newer approved version.DiffThis version (03 Oct 2018 08:38) was approved by Pranit Jadhav.The Previously approved version (25 Sep 2018 13:31) is available.Diff

This is an old revision of the document!


EV-COG-ADF7023-9Z User Guide

EV-COG-ADF7023-9Z is an evaluation board to evaluate the ADF7023-J High Performance, Low Power, 902-958MHz ISM Band FSK/GFSK/MSK/GMSK transceiver IC. The EV-COG-AD3029LZ MCU Cog board controls ADF7023-J daughter boards. The daughter board plugs directly into the MCU Cog to provide a full ADF7023-J development kit for a wide range of applications depending upon the daughterboard selection.

Features

  • Directly plugs in to EV-COG-AD3029LZ MCU Cog Board.
  • SMA (female type) connector for Whip Antenna.
  • Chip antenna available if Whip Antenna is not used.
  • Power through MCU Cog board. No external power supply required.

Interface

EV-COG-ADF7023-9Z connects to MCU Cog through a hirose connector available on the daughter board. The MCU Cog will power up the daughter board, so no other external power supply is required. The daughter board has a testport P2 which can be used to probe logic analyzer to the GPIOs connecting MCU Cog to ADF7023-J.

Primary Side

Secondary Side

Test Port

Schematics, PCB Layout, Bill of Material

resources/eval/user-guides/ev-cog-adf7023-9z.1538548665.txt.gz · Last modified: 03 Oct 2018 08:37 by Pranit Jadhav