This is an old revision of the document!
EV-COG-ADF7023-9Z is an evaluation board to evaluate the ADF7023-J High Performance, Low Power, ISM Band FSK/GFSK/MSK/GMSK transceiver IC. The EV-COG-AD3029LZ evaluation board is a motherboard that controls ADF7023-J daughter boards. The daughter board plugs directly into the motherboard to provide a full ADF7023-J development kit for a wide range of applications depending upon the daughterboard selection. The various available daughter boards can be selected from the following Table 1.
EV-COG-ADF7023-9Z connects to motherboard through a hirose connector available on the daughter board. The motherboard will power up the daughter board, so no other external power supply is required. The daughter board has a testport P2 which can be used to probe logic analyzer to the GPIOs connecting MCU on the motherboard to ADF7023-J.