EV-COG-AD4050WZ with IAR Embedded Workbench for ARM
There are no seperate toolchain,On-Board Peripheral Drivers & Software for EV-COG-AD4050WZ, the toolchain,On-Board Peripheral Drivers & Software for EV-COG-AD4050LZ works with EV-COG-AD4050WZ.The user needs to change only the pin muxing based on the application.For help regarding pinmapping refer to the Hardware Details section.
IDE Setup
Install IAR Embedded Workbench for ARM
Please visit
https://www.iar.com/ to download IAR Embedded Workbench for ARM (version 8.20.1 or above).
License Installation
Software Packs and Driver Setup
Download the following packs for EV-COG-AD4050LZ
Start IAR Embedded Workbench for ARM.
Go to Project→ CMSIS-Pack→ Pack Installer.
In
'CMSIS Pack Manager' window, click 'Install local pack file'.
In 'Pack file to install' window navigate to the downloaded pack (as already done in step 1 of this section), select all the packs to install and click Open.
Running an Example Project
The pins for LEDs and BUTTONs are different in example project as they are developed for LZ version of 4050.So before running the example in your WZ board change the pinmuxing appropriately by looking at the hardware details section.
Power the MCU Cog using a
USB (micro-B) Cable. You should see a red LED and a yellow LED turn on by default.
In IAR
IDE, go to Project→ Create New Project…
In
'Create New Project' window, Select
'CMSIS Pack Example' and click 'OK'.
Expand Analog Devices, select
ADuCM4050 and click 'Next'.
Select
button_press example and click 'Finish'.
Save the project to the desired location.
Click on 'Debug and Download' icon
on the menu bar. This will compile, build and download the project on EV-COG-AD4050LZ using CMSIS-DAP.
Click on 'Run' icon
to start the debug session.
Now press BTN1 or BTN2 on EV-COG-AD4050LZ and inspect corresponding LED
You are all set!
Back
End Document