Wiki

This version (03 Sep 2018 07:50) was approved by Gowtham shanmugaraj.The Previously approved version (03 Sep 2018 07:44) is available.Diff

MCU Cog Quick Start Guide

There are no seperate toolchain,On-Board Peripheral Drivers & Software for EV-COG-AD4050WZ, the toolchain,On-Board Peripheral Drivers & Software for EV-COG-AD4050LZ works with EV-COG-AD4050WZ.The user needs to change only the pin muxing based on the application.For help regarding pinmapping refer to the Hardware Details section.

Setting up EV-COG-AD4050WZ is a three step process.

  1. IDE Setup
  2. Software Packs & Drivers Setup
  3. Running an Example Project


EV-COG-AD4050WZ can be used with following Toolchains. Please see below links for the quickstart guide with respect to different IDEs.

CrossCore Embedded Studio

Click below link to go to CrossCore Embedded Studio userguide.

EV-COG-AD4050WZ with CrossCore Embedded Studio

IAR Embedded Workbench for ARM

Click below link to go to CrossCore Embedded Studio userguide.

EV-COG-AD4050WZ with IAR Embedded Workbench for ARM

Back


End Document

resources/eval/user-guides/ev-cog-ad4050w/quickstart.txt · Last modified: 03 Sep 2018 07:48 by Gowtham shanmugaraj