Wiki

This version is outdated by a newer approved version.DiffThis version (03 Sep 2018 07:55) was approved by Gowtham shanmugaraj.

This is an old revision of the document!


Hardware Details

This page contains hardware-related information about the EV-COG-AD3029WZ board and the various hardware add on modules which can be used with the board. Each sub-section contains a detailed description of the board, connectors, jumpers and buttons. It also provides links to the Schematics, Bill of materials, design projects, and Technical documentation. It also gives internal links to the provided example demo software projects.

The following boards are currently available:


End Document

Back

resources/eval/user-guides/ev-cog-ad4050w/hw_details.1535954105.txt.gz · Last modified: 03 Sep 2018 07:55 by Gowtham shanmugaraj