Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

resources:eval:user-guides:ev-cog-ad4050w:hw_details [03 Sep 2018 07:55] – created Gowtham shanmugarajresources:eval:user-guides:ev-cog-ad4050w:hw_details [11 Sep 2018 09:44] (current) – changed 3029 to 4050 Gowtham shanmugaraj
Line 1: Line 1:
 ====== Hardware Details ====== ====== Hardware Details ======
-This page contains hardware-related information about the EV-COG-AD3029WZ board and the various hardware add on modules which can be used with the board. Each sub-section contains a detailed description of the board, connectors, jumpers and buttons. It also provides links to the Schematics, Bill of materials, design projects, and Technical documentation. It also gives internal links to the provided example demo software projects. +This page contains hardware-related information about the EV-COG-AD4050WZ board and the various hardware add on modules which can be used with the board. Each sub-section contains a detailed description of the board, connectors, jumpers and buttons. It also provides links to the Schematics, Bill of materials, design projects, and Technical documentation. It also gives internal links to the provided example demo software projects. 
  
 The following boards are currently available:  The following boards are currently available: 
resources/eval/user-guides/ev-cog-ad4050w/hw_details.txt · Last modified: 11 Sep 2018 09:44 by Gowtham shanmugaraj