Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |
resources:eval:user-guides:ev-cog-ad4050w:cog_hw_userguide [03 Jan 2021 21:46] – fix links Robin Getz | resources:eval:user-guides:ev-cog-ad4050w:cog_hw_userguide [14 Jan 2021 05:24] (current) – use / interwiki links Robin Getz |
---|
===== Wireless Connectivity Options ===== | ===== Wireless Connectivity Options ===== |
| |
The MCU Cog board offers support for ADI RF daughter-cards such as the EV-ADF70301-915AZ via the "EV-COG-BLEINTP1" connectivity Cog board that can be attached at Connector P2. This connectivity Cog board also has on-board BTLE circuit enabling the MCU Cog board to use BTLE communication as well. More details regarding wireless connectivity options are available on the [[https://wiki.analog.com/resources/eval/user-guides/ev-cog-bleintp1z|EV-COG-BLEINTP1 Wiki page]]. | The MCU Cog board offers support for ADI RF daughter-cards such as the EV-ADF70301-915AZ via the "EV-COG-BLEINTP1" connectivity Cog board that can be attached at Connector P2. This connectivity Cog board also has on-board BTLE circuit enabling the MCU Cog board to use BTLE communication as well. More details regarding wireless connectivity options are available on the [[/resources/eval/user-guides/ev-cog-bleintp1z|EV-COG-BLEINTP1 Wiki page]]. |
| |
<note important>UART1 is wired to RF Module. If an application wants to use UART1 for some purpose other than RF module, then RF Module cannot be used. | <note important>UART1 is wired to RF Module. If an application wants to use UART1 for some purpose other than RF module, then RF Module cannot be used. |