Wiki

This version is outdated by a newer approved version.DiffThis version (19 Apr 2021 09:00) was approved by Jeric Vargas.The Previously approved version (03 Jan 2021 22:04) is available.Diff

This is an old revision of the document!


EV-COG-AD4050 Development Kit

The EV-COG-AD4050 (referred also as MCU Cog) is a development platform based on the industry leading ultra low power ADuCM4050 32-bit ARM Cortex™-M4F microcontroller. The platform is designed to be a development and prototyping vehicle to get customer ideas from concept to production with a minimal risk and faster time to market.
Applications using EV-COG-AD4050 board can be developed using one of the following toolchains.

  1. Crosscore Embedded Studio 2.7.0 and above - an Eclipse based Analog Devices Interactive Development Environment.
  2. IAR Embedded Workbench for ARM 8.20 and above
  3. Keil uVision 4 and above
  4. ARM mbed Compiler

Make sure a valid license for the selected toolchain is installed before using EV-COG-AD4050 board.

  1. Software Packs & Board Support Package:EV-COG-AD4050 software architecture is categorized into 2 groups as below.
resources/eval/user-guides/ev-cog-ad4050lz.1618815624.txt.gz · Last modified: 19 Apr 2021 09:00 by Jeric Vargas