Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Next revision
Previous revision
resources:eval:user-guides:ev-cog-ad4050lz:tools_driver [12 Aug 2017 09:43]
Pranit Jadhav
resources:eval:user-guides:ev-cog-ad4050lz:tools_driver [22 May 2018 13:48]
Gowtham shanmugaraj .
Line 1: Line 1:
 ====== Tools and Driver Details ====== ====== Tools and Driver Details ======
 +
 +<note >There are no seperate toolchain,​On-Board Peripheral Drivers & Software for EV-COG-AD4050WZ,​ the toolchain,​On-Board Peripheral Drivers & Software for EV-COG-AD4050LZ works with EV-COG-AD4050WZ.The user needs to change only the pin muxing based on the application.For help regarding pinmapping refer to the Hardware Details section.
 +</​note>​
  
 This chapter provides all the necessary steps to download, install, and setup the software environment from Analog Devices. ​ There is also information on the different USB modes and drivers needed. ​ This chapter provides all the necessary steps to download, install, and setup the software environment from Analog Devices. ​ There is also information on the different USB modes and drivers needed. ​
Line 5: Line 8:
 It contains two main sections: It contains two main sections:
  
-   - **[[resources:​eval:​user-guides:​ev-cog-ad4050lz:​tools:​cces_download|CrossCore Embedded Studio Download & Install]]** - Provides all the necessary instructions on how to download and install the CrossCore Embedded Studios software development environment. +   - **[[resources:​eval:​user-guides:​ev-cog-ad4050wz:​tools:​cces_download|CrossCore Embedded Studio Download & Install]]** - Provides all the necessary instructions on how to download and install the CrossCore Embedded Studios software development environment. 
-       * **[[resources:​ev:​user-guides:​ev-cog-ad4050lz:​tools:​cces_guide|CrossCore Embedded Studio Quickstart Userguide]]** - Provides information about using the CrossCore Embedded Studios IDE, in particular, the process of importing, building, debugging, and creating user applications for the EV-COG-AD4050LZ.+       * **[[resources:​ev:​user-guides:​ev-cog-ad4050wz:​tools:​cces_guide|CrossCore Embedded Studio Quickstart Userguide]]** - Provides information about using the CrossCore Embedded Studios IDE, in particular, the process of importing, building, debugging, and creating user applications for the EV-COG-AD4050LZ.
    - **[[resources:​eval:​user-guides:​ev-cog-ad4050lz:​tools:​hardware_usb|Driver Installation for On-board Debugger (CMSIS DAP)]]** - Provides detailed information how to load pre-compiled .HEX or .BIN files using the USB drive of the EV-COG-AD4050LZ board.    - **[[resources:​eval:​user-guides:​ev-cog-ad4050lz:​tools:​hardware_usb|Driver Installation for On-board Debugger (CMSIS DAP)]]** - Provides detailed information how to load pre-compiled .HEX or .BIN files using the USB drive of the EV-COG-AD4050LZ board.
   ​   ​
resources/eval/user-guides/ev-cog-ad4050lz/tools_driver.txt · Last modified: 22 May 2018 13:48 by Gowtham shanmugaraj