Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |
resources:eval:user-guides:ev-cog-ad4050lz:tools_driver [14 May 2018 12:26] – . Gowtham shanmugaraj | resources:eval:user-guides:ev-cog-ad4050lz:tools_driver [22 May 2018 13:48] (current) – . Gowtham shanmugaraj |
---|
====== Tools and Driver Details ====== | ====== Tools and Driver Details ====== |
| |
<note important>There is no seperate toolchain,DFP,BSP for EV-COG-AD4050WZ, the toolchain,DFP,BSP for EV-COG-AD4050LZ works with EV-COG-AD4050WZ.The user needs to change only the pin muxing based on his/her application.For help regarding pinmapping refer to the Hardware Details section. | <note >There are no seperate toolchain,On-Board Peripheral Drivers & Software for EV-COG-AD4050WZ, the toolchain,On-Board Peripheral Drivers & Software for EV-COG-AD4050LZ works with EV-COG-AD4050WZ.The user needs to change only the pin muxing based on the application.For help regarding pinmapping refer to the Hardware Details section. |
</note> | </note> |
| |
This chapter provides all the necessary steps to download, install, and setup the software environment from Analog Devices. There is also information on the different USB modes and drivers needed. | This chapter provides all the necessary steps to download, install, and setup the software environment from Analog Devices. There is also information on the different USB modes and drivers needed. |
| |