This is an old revision of the document!
The ADuCM4x50 Device Family Pack (DFP) provides access to all the necessary on-chip peripheral drivers for ADuCM4050 devices. This software layer is the foundation layer needed when writing applications using this microprocessor family. When combined with the EV-COG-AD4050LZ software pack as well as the Sensors software pack, there are many great Internet of Things(IoT) applications and demos that can be replicated using the EV-COG-AD4050LZ development platform.
The following on-chip drivers are provided as part of the ADuCM4x50 Device Family Pack:
For detailed information regarding the ADuCM4x50 DFP, please see our complete ADuCM4x50 software user guide.
You MUST have this software package installed on your laptop or PC in order to compile, debug, and run the applications for the EV-COG-AD4050LZ platform.
The software pack can be installed directly by the tool chain's CMSIS pack manager. Optionally, you may download and then use the CMSIS pack manager's manual installation to install the pack.
End of Document