Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Next revision
Previous revision
resources:eval:user-guides:ev-cog-ad4050lz:help_support [12 Aug 2017 09:38]
Pranit Jadhav [What to do When Things Go Wrong]
resources:eval:user-guides:ev-cog-ad4050lz:help_support [03 Jan 2021 22:04] (current)
Robin Getz fix links
Line 1: Line 1:
 ====== Help and Support ====== ====== Help and Support ======
 +
 +<note >There are no seperate toolchain,​On-Board Peripheral Drivers & Software for EV-COG-AD4050WZ,​ the toolchain,​On-Board Peripheral Drivers & Software for EV-COG-AD4050LZ works with EV-COG-AD4050WZ.The user needs to change only the pin muxing based on the application.For help regarding pinmapping refer to the Hardware Details section.
 +</​note>​
  
 Do you need help or have general support questions, than I hope this page helps you resolve those.  ​ Do you need help or have general support questions, than I hope this page helps you resolve those.  ​
Line 17: Line 20:
     * The first thing to try in this case, is to [[resources:​eval:​user-guides:​ev-cog-ad4050lz:​tools:​hardware_usb|drag and drop]] a known good .HEX or .BIN program into flash.(something with quick visible indicators works best)     * The first thing to try in this case, is to [[resources:​eval:​user-guides:​ev-cog-ad4050lz:​tools:​hardware_usb|drag and drop]] a known good .HEX or .BIN program into flash.(something with quick visible indicators works best)
     * If drag and drop is not working, it may be necessary to erase the flash. To do so:  ​     * If drag and drop is not working, it may be necessary to erase the flash. To do so:  ​
-      - Download and install the CrossCore Serial Flash Programmer from here: [[http://​www.analog.com/​en/​design-center/​processors-and-dsp/​evaluation-and-development-software/​crosscore-serial-flash-programmer.html#​dsp-overview]].  ​+      - Download and install the CrossCore Serial Flash Programmer from here: [[adi>en/​design-center/​processors-and-dsp/​evaluation-and-development-software/​crosscore-serial-flash-programmer.html#​dsp-overview]].  ​
       - Make sure that the USB is connected and on UART header (P8) 1 & 2 and 7 & 8 are shorted. ​       - Make sure that the USB is connected and on UART header (P8) 1 & 2 and 7 & 8 are shorted. ​
       - Power cycle the EV-COG-AD4050LZ board while holding down the boot switch. ​       - Power cycle the EV-COG-AD4050LZ board while holding down the boot switch. ​
resources/eval/user-guides/ev-cog-ad4050lz/help_support.1502523499.txt.gz · Last modified: 12 Aug 2017 09:38 by Pranit Jadhav