Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Next revision
Previous revision
resources:eval:user-guides:ev-cog-ad4050lz:help_support [12 Aug 2017 09:28]
Pranit Jadhav [CrossCore Embedded Studio questions]
resources:eval:user-guides:ev-cog-ad4050lz:help_support [03 Jan 2021 22:04] (current)
Robin Getz fix links
Line 1: Line 1:
 ====== Help and Support ====== ====== Help and Support ======
 +
 +<note >There are no seperate toolchain,​On-Board Peripheral Drivers & Software for EV-COG-AD4050WZ,​ the toolchain,​On-Board Peripheral Drivers & Software for EV-COG-AD4050LZ works with EV-COG-AD4050WZ.The user needs to change only the pin muxing based on the application.For help regarding pinmapping refer to the Hardware Details section.
 +</​note>​
  
 Do you need help or have general support questions, than I hope this page helps you resolve those.  ​ Do you need help or have general support questions, than I hope this page helps you resolve those.  ​
Line 15: Line 18:
   - Program the EV-COG-AD4050LZ   - Program the EV-COG-AD4050LZ
     * Sometimes a flashed program doesn'​t run properly or can make it difficult to run the debugger. ​     * Sometimes a flashed program doesn'​t run properly or can make it difficult to run the debugger. ​
-    * The first thing to try in this case, is to [[resources:​eval:​user-guides:​eval-cog-ad4050lz:​tools:​hardware_usb|drag and drop]] a known good .HEX or .BIN program into flash.(something with quick visible indicators works best)+    * The first thing to try in this case, is to [[resources:​eval:​user-guides:​ev-cog-ad4050lz:​tools:​hardware_usb|drag and drop]] a known good .HEX or .BIN program into flash.(something with quick visible indicators works best)
     * If drag and drop is not working, it may be necessary to erase the flash. To do so:  ​     * If drag and drop is not working, it may be necessary to erase the flash. To do so:  ​
-      - Download and install the CrossCore Serial Flash Programmer from here: [[http://​www.analog.com/​en/​design-center/​processors-and-dsp/​evaluation-and-development-software/​crosscore-serial-flash-programmer.html#​dsp-overview]].  ​+      - Download and install the CrossCore Serial Flash Programmer from here: [[adi>en/​design-center/​processors-and-dsp/​evaluation-and-development-software/​crosscore-serial-flash-programmer.html#​dsp-overview]].  ​
       - Make sure that the USB is connected and on UART header (P8) 1 & 2 and 7 & 8 are shorted. ​       - Make sure that the USB is connected and on UART header (P8) 1 & 2 and 7 & 8 are shorted. ​
       - Power cycle the EV-COG-AD4050LZ board while holding down the boot switch. ​       - Power cycle the EV-COG-AD4050LZ board while holding down the boot switch. ​
       - Select the mbed serial COM port in the CrossCore Serial Flash Programmer, and erase the flash.       - Select the mbed serial COM port in the CrossCore Serial Flash Programmer, and erase the flash.
-      - Then try [[resources:​eval:​user-guides:​eval-cog-ad4050lz:​tools:​hardware_usb|drag and drop]] a .HEX or .BIN file into flash+      - Then try [[resources:​eval:​user-guides:​ev-cog-ad4050lz:​tools:​hardware_usb|drag and drop]] a .HEX or .BIN file into flash
     * If the mass erase didn't work, and you are trying to drag and drop a large .BIN file on EV-COG-AD4050LZ hardware, it's possible that the mbed interface file needs to be updated to support your application.     * If the mass erase didn't work, and you are trying to drag and drop a large .BIN file on EV-COG-AD4050LZ hardware, it's possible that the mbed interface file needs to be updated to support your application.
-      - Please visit the [[resources:​eval:​user-guides:​eval-cog-ad4050lz:​tools:​hardware_usb|Driver Installation for On-board Debugger (CMSIS DAP)]] page in order to put the board in update mode. +      - Please visit the [[resources:​eval:​user-guides:​ev-cog-ad4050lz:​tools:​hardware_usb|Driver Installation for On-board Debugger (CMSIS DAP)]] page in order to put the board in update mode. 
-      - Once you are in "​maintenance mode" you should drag and drop the latest interface file onto your maintenance drive. ​ That file can be downloaded at the bottom of [[resources:​eval:​user-guides:​eval-cog-ad4050lz:​tools:​hardware_usb|Driver Installation for On-board Debugger (CMSIS DAP)]].+      - Once you are in "​maintenance mode" you should drag and drop the latest interface file onto your maintenance drive. ​ That file can be downloaded at the bottom of [[resources:​eval:​user-guides:​ev-cog-ad4050lz:​tools:​hardware_usb|Driver Installation for On-board Debugger (CMSIS DAP)]].
   - Not receiving/​transmitting data to the UART   - Not receiving/​transmitting data to the UART
     * Make sure that the UART header (P8) is positioned in the correct destination to transmit/​receive UART data.     * Make sure that the UART header (P8) is positioned in the correct destination to transmit/​receive UART data.
   ​   ​
 This is just a brief self-help guide to troubleshooting common issues. ​ If you have other questions that need answering please direct those requests to the locations outlined below. This is just a brief self-help guide to troubleshooting common issues. ​ If you have other questions that need answering please direct those requests to the locations outlined below.
 +
 +
  
 ===== Hardware, Software, and Documentation Questions ===== ===== Hardware, Software, and Documentation Questions =====
resources/eval/user-guides/ev-cog-ad4050lz/help_support.1502522913.txt.gz · Last modified: 12 Aug 2017 09:28 by Pranit Jadhav