This shows you the differences between two versions of the page.
Both sides previous revision Previous revision | |||
resources:eval:user-guides:ev-cog-ad3029wz:quickstart_1 [12 Sep 2018 07:58] Gowtham shanmugaraj [Keil uVision IDE] |
resources:eval:user-guides:ev-cog-ad3029wz:quickstart_1 [12 Sep 2018 08:35] Gowtham shanmugaraj . |
||
---|---|---|---|
Line 1: | Line 1: | ||
====== MCU Cog Quick Start Guide ====== | ====== MCU Cog Quick Start Guide ====== | ||
- | <note >There are no seperate toolchain,On-Board Peripheral Drivers & Software for EV-COG-AD3029WZ, the toolchain,On-Board Peripheral Drivers & Software for EV-COG-AD3029LZ works with EV-COG-AD3029WZ.The user needs to change only the pin muxing based on the application.For help regarding pinmapping refer to the Hardware Details section. | + | <note > **There are no seperate toolchain,On-Board Peripheral Drivers & Software for EV-COG-AD3029WZ, the toolchain,On-Board Peripheral Drivers & Software for EV-COG-AD3029LZ works with EV-COG-AD3029WZ.The user needs to change only the pin muxing based on the application.For help regarding pinmapping refer to the Hardware Details section.** |
</note> | </note> | ||