This is an old revision of the document!
Software Packs & Board Support Package
There are no seperate toolchain,On-Board Peripheral Drivers & Software for EV-COG-AD3029WZ, the toolchain,On-Board Peripheral Drivers & Software for EV-COG-AD3029LZ works with EV-COG-AD3029WZ.The user needs to change only the pin muxing based on the application.For help regarding pinmapping refer to the Hardware Details section.
A modular software framework is provided for quick application prototyping. Based on the application use case, developers need to download the respective software packs.
Please make sure you install either of the below toolchain before installing any of the below packs
IAR Embedded Workbench for ARM 8.20.1 or higher
CrossCore Embedded Studio 2.7.0 ® or higher
packs
The Cog software development kit consists of these packs
-
Version: 3.1.0 - Extended support for IAR Embedded Workbench and Keil uVision. [Latest]
Version: 2.0.0 -
API Changes to suit IoT applications
Version: 1.0.6 - Support Release
Version: 1.0.5 - Enables ECC during flash programming
-
Version 3.1.0 - Extended support for IAR Embedded Workbench.[Latest]
Version: 1.0.0 - Initial Release
-
Version: 1.1.0 - Move example projects to respective board support packages. [Latest]
Version: 1.0.0 - Initial Release
-
Version: 1.0.0 - Initial Release [Latest]
Back
End of Document