Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
resources:eval:user-guides:ev-cog-ad3029wz:packs_bsp [17 Sep 2018 09:08] – . Gowtham shanmugarajresources:eval:user-guides:ev-cog-ad3029wz:packs_bsp [17 Sep 2018 09:13] (current) – . Gowtham shanmugaraj
Line 12: Line 12:
  
 The Cog software development kit consists of these packs The Cog software development kit consists of these packs
-   - [[resources:eval:user-guides:ev-cog-ad3029lz:software:aducm302x|Analog Devices ADuCM302x Device Support Packs]] - This is a bare minimum pack required to enable working with ADuCM3029 and develop simple applications using the on-chip drivers.+   - [[resources:eval:user-guides:ev-cog-ad3029wz:software:aducm302x|Analog Devices ADuCM302x Device Support Packs]] - This is a bare minimum pack required to enable working with ADuCM3029 and develop simple applications using the on-chip drivers.
         * //Version History//                * //Version History//       
          - **Version: 3.1.0** - Extended support for IAR Embedded Workbench and Keil uVision. **[Latest]**          - **Version: 3.1.0** - Extended support for IAR Embedded Workbench and Keil uVision. **[Latest]**
Line 18: Line 18:
          - Version: 1.0.6 - Support Release          - Version: 1.0.6 - Support Release
          - Version: 1.0.5 - Enables ECC during flash programming          - Version: 1.0.5 - Enables ECC during flash programming
-   - [[resources:eval:user-guides:ev-cog-ad3029lz:software:ev-cog-ad3029lz| Analog Devices EV-COG-AD3029LZ Off-Chip Drivers and Examples]] - This pack along with the DFP is required to develop applications using the on-board drivers.+   - [[resources:eval:user-guides:ev-cog-ad3029wz:software:ev-cog-ad3029wz| Analog Devices EV-COG-AD3029WZ Off-Chip Drivers and Examples]] - This pack along with the DFP is required to develop applications using the on-board drivers.
         * //Version History//          * //Version History// 
          - **Version 3.1.0** - Extended support for IAR Embedded Workbench.**[Latest]**          - **Version 3.1.0** - Extended support for IAR Embedded Workbench.**[Latest]**
resources/eval/user-guides/ev-cog-ad3029wz/packs_bsp.txt · Last modified: 17 Sep 2018 09:13 by Gowtham shanmugaraj