Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
resources:eval:user-guides:ev-cog-ad3029wz:cog_hw_userguide [03 Jan 2021 21:46] – fix links Robin Getzresources:eval:user-guides:ev-cog-ad3029wz:cog_hw_userguide [14 Jan 2021 05:24] (current) – use / interwiki links Robin Getz
Line 66: Line 66:
 ===== Wireless Connectivity Options ===== ===== Wireless Connectivity Options =====
  
-The MCU Cog board offers support for ADI RF daughter-cards such as the EV-ADF70301-915AZ via the "EV-COG-BLEINTP1" connectivity Cog board that can be attached at Connector P2. This connectivity Cog board also has on-board BTLE circuit enabling the MCU Cog board to use BTLE communication as well. More details regarding wireless connectivity options are available on the [[https://wiki.analog.com/resources/eval/user-guides/ev-cog-bleintp1z|EV-COG-BLEINTP1 Wiki page]].+The MCU Cog board offers support for ADI RF daughter-cards such as the EV-ADF70301-915AZ via the "EV-COG-BLEINTP1" connectivity Cog board that can be attached at Connector P2. This connectivity Cog board also has on-board BTLE circuit enabling the MCU Cog board to use BTLE communication as well. More details regarding wireless connectivity options are available on the [[/resources/eval/user-guides/ev-cog-bleintp1z|EV-COG-BLEINTP1 Wiki page]].
  
 ===== Buttons/LED(s) ===== ===== Buttons/LED(s) =====
resources/eval/user-guides/ev-cog-ad3029wz/cog_hw_userguide.txt · Last modified: 14 Jan 2021 05:24 by Robin Getz