Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
resources:eval:user-guides:ev-cog-ad3029lz:tools:cces_guide [27 Mar 2018 12:56] – [How to install Packs for CCES] Pranit Jadhavresources:eval:user-guides:ev-cog-ad3029lz:tools:cces_guide [11 Sep 2018 08:18] (current) – . Gowtham shanmugaraj
Line 1: Line 1:
-====== Cross Core Embedded Studio Quickstart User Guide for EV-COG-AD3029LZ======+====== Cross Core Embedded Studio Quickstart User Guide for EV-COG-AD3029WZ====== 
 +<note>There is no separate tool chain or software packs for EV-COG-AD3029WZ, the tool chain and software packs for EV-COG-AD3029LZ is compatible with EV-COG-AD3029WZ, except some pin map changes</note>
  
 This page describes how to use the ADuCM302x Device Family Pack (DFP) with CrossCore Embedded Studio (CCES) to create, import, build and debug applications for the ADuCM302x processor. The ADuCM302x MCU integrates an ARM Cortex-M3 processor with various on-chip peripherals within a single package. This page describes how to use the ADuCM302x Device Family Pack (DFP) with CrossCore Embedded Studio (CCES) to create, import, build and debug applications for the ADuCM302x processor. The ADuCM302x MCU integrates an ARM Cortex-M3 processor with various on-chip peripherals within a single package.
Line 5: Line 6:
 <note>ADuCM302x family has two versions of the device, ADuCM3027 and ADuCM3029, the DFP supports both these versions</note> <note>ADuCM302x family has two versions of the device, ADuCM3027 and ADuCM3029, the DFP supports both these versions</note>
  
-This page describes how to install and work with the Analog Devices ADuCM302x DFP to start developing applications for the EV-COG-AD3029LZ.+This page describes how to install and work with the Analog Devices ADuCM302x DFP to start developing applications for the EV-COG-AD3029WZ.
  
 Additional help documentation can be found by opening CCES and selecting "Help Contents" from the CCES Help menu. Additional help documentation can be found by opening CCES and selecting "Help Contents" from the CCES Help menu.
Line 63: Line 64:
  
 ==== ADuCM3029 Board Support Packs (BSP) ==== ==== ADuCM3029 Board Support Packs (BSP) ====
-=== EV-COG-AD3029LZ Board Support Pack ===+=== EV-COG-AD3029WZ/LZ Board Support Pack ===
  
 The EV-COG-AD3029LZ Board Support Pack (BSP) provides the drivers for off-chip peripherals which are on the EV-COG-AD3029LZ Evaluation Board and examples for peripherals on the ADcCM3029 processor. The drivers and examples in the BSP are designed to work with CrossCore Embedded Studio and the ADuCM302x Device Family Pack (DFP).  The EV-COG-AD3029LZ Board Support Pack (BSP) provides the drivers for off-chip peripherals which are on the EV-COG-AD3029LZ Evaluation Board and examples for peripherals on the ADcCM3029 processor. The drivers and examples in the BSP are designed to work with CrossCore Embedded Studio and the ADuCM302x Device Family Pack (DFP). 
Line 71: Line 72:
 ==== ADI Sensor Software Pack ==== ==== ADI Sensor Software Pack ====
  
-The ADI Sensor Software pack contains various sensor software components and associated examples. The examples in the sensor pack are designed to work with EV-COG-AD3029LZ board and associated sensor shields. ADI Sensor Software requires CrossCore Embedded Studio (CCES), ADuCM302x Device Family Pack (DFP) and EV-COG-AD3029LZ Board Support Pack (BSP).+The ADI Sensor Software pack contains various sensor software components and associated examples. The examples in the sensor pack are designed to work with EV-COG-AD3029WZ board and associated sensor shields. ADI Sensor Software requires CrossCore Embedded Studio (CCES), ADuCM302x Device Family Pack (DFP) and EV-COG-AD3029LZ Board Support Pack (BSP).
  
 For more information on the ADI Sensor Software Pack, please refer to the User's Guide in the Documents folder (e.g. C:\Analog Devices\CrossCore Embedded Studio 2.6.0\ARM\packs\AnalogDevices\ADI-SensorSoftware\1.0.0\Documents\SensorSoftware_Users_Guide.pdf) For more information on the ADI Sensor Software Pack, please refer to the User's Guide in the Documents folder (e.g. C:\Analog Devices\CrossCore Embedded Studio 2.6.0\ARM\packs\AnalogDevices\ADI-SensorSoftware\1.0.0\Documents\SensorSoftware_Users_Guide.pdf)
resources/eval/user-guides/ev-cog-ad3029lz/tools/cces_guide.txt · Last modified: 11 Sep 2018 08:18 by Gowtham shanmugaraj