Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Last revisionBoth sides next revision |
resources:eval:user-guides:ev-cog-ad3029lz:software:sensor [04 Oct 2017 07:25] – [Downloading the Sensor Software Pack] Pranit Jadhav | resources:eval:user-guides:ev-cog-ad3029lz:software:sensor [13 Nov 2017 07:07] – Pranit Jadhav |
---|
====== Sensor Application Software Packs and Drivers ====== | ====== Analog Devices Sensor Drivers and Examples====== |
===== General Description/Overview ===== | ===== General Description/Overview ===== |
Sensor software pack contains sensor software components. Sensor components are based on the sensor classes which abstract the functionality across sensor types. The Sensors software pack provides access to all the necessary add-on module digital drivers that attach to the [[ADI>EV-COG-AD3029LZ]] development platform. This software layer is the highest layer of abstraction from the microprocessor, and because of this can be useful to jump start code development for your application using any microprocessor. For example, if you are using the ADXL362, the Sensor software pack contains drivers and code snippets on the application level, so that can be transported to other microprocessor, with confidence that Analog Devices provided the application framework pieces. When combined with the [[adi>ADuCM3029]] and [[adi>EV-COG-AD3029LZ]] software packs there are many great Internet of Things(IoT) applications. | Sensor software pack contains sensor software components. Sensor components are based on the sensor classes which abstract the functionality across sensor types. The Sensors software pack provides access to all the necessary add-on module digital drivers that attach to the [[ADI>EV-COG-AD3029LZ]] development platform. This software layer is the highest layer of abstraction from the microprocessor, and because of this can be useful to jump start code development for your application using any microprocessor. For example, if you are using the ADXL362, the Sensor software pack contains drivers and code snippets on the application level, so that can be transported to other microprocessor, with confidence that Analog Devices provided the application framework pieces. When combined with the [[adi>ADuCM3029]] and [[adi>EV-COG-AD3029LZ]] software packs there are many great Internet of Things(IoT) applications. |